hello all, just wanted to really quick explain my setup and what im trying to do then i can get into details later
i have built this robot thats can be controlled via ad-hoc or over the internet WI-Fi, from a laptop, PSP, PDA, Wiimote, things like that. the robot has fully on board windows XP with supporting hardware. im using the Roboteq AX2550 brushed DC motor controller.
now for the paintball part, im using a Sypder E99, which is half electric and half mechanical. i have already made the gun where i can fire it over the internet via a relay board, but thats just for now. i want to put the marker on top of the robot and make a paintball turret. i been looking and reading around for a few days now. i want to use the
4-Servo Phidget USB Servo Controller
with 2 of these servos off Ebay
i was wondering if the Phidget board will be able to handle those servos?
a neat note to add im hooking the Phidget board up to image processing software called RoboRealm everyone should check it out its very neat!!
Project log found at Bit-tech.net Semi-teQ
im open to any ideas question or concerns, thanks in advanced!



Reply With Quote




Bookmarks