Results 1 to 2 of 2

Thread: Easy Programing of servos and play back

  1. #1

    Easy Programing of servos and play back

    For beginners at serovo programing like me i found a new board called
    ServoCity 4-Servo Recorder/Playback Controller


    Introducing the new ServoCity 4-Servo Recorder/Playback Controller. This unit allows you to operate 4 servos one at a time or simultaneously. Each knob will control your servos up to 180°. Simply plug in a battery or regulated power supply, plug in your servos, rotate the corresponding knobs and your servos will move proportionally to the knob movement. Once you are ready to record the movements, slide the selector switch over to record and then move the servos again. The internal memory stores all the servos motions and even the delay time between motions. Once you have recorded the movements and are ready to play them back, use the selector switch to choose between single or loop mode. Single mode will play the movements back once, loop mode will continuously play back the movements. All the servos can operate at the same time and the program can easily be changed. Since your program is stored on a chip, power is not required to maintain the program. Perfect for animation, robotic projects, pan and tilt systems or wherever you need the exact same movement each time. The unit will handle 4 servos simultaneously and will work with analog or digital servos.
    Each knob is labeled as to which servo it operates. Move a knob fast and the servo will move fast, move it slowly and the servo will move slowly. In record mode it even records the time. Move the servo every 18 seconds, and in playback mode the servo will move every 18 seconds since it even records delays between servo movements. It records and plays back the exact speed, time and range of motion for each servo even at the same time.

  2. #2
    Join Date
    Sep 2006
    Location
    Chicago Illinois
    Posts
    682
    Images
    174
    Rep Power
    85

    Re: Easy Programing of servos and play back

    That does look like a handy unit. We are so used to using serial & USB based controllers around here that nearly everything we do ends up involving a computer and writing a program! Talk about over engineering in some cases. It would be handy to have this tool for quick and dirty mockups. Thanks for the heads up for others to know about it.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •