Results 1 to 3 of 3

Thread: Go-to Airsoft weaponry solution?

  1. #1
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Go-to Airsoft weaponry solution?

    Sorry for the lazy post, I promise I squinted long and hard for a good 4 seconds at the forum before asking:

    Has there been any general consensus or open sourced design for airsoft weapons? Or are most competitors still using their own custom designs?

    Was floating around the idea of designing something that can easily be built around a standard AEG mechbox + printed parts for hopper/mag.

    Also, any good sources for barrels?

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: Go-to Airsoft weaponry solution?

    jwatte had a design built around a fairly standard AEG on Shapeways, but not sure it is still available from there. It also had a tiny hopper stirring motor and slot for an optointerrupter to verify something about the state of the loading/firing action. Thinking the design was able to accommodate any barrel/hopup. Given my proximity, Airsoft Atlanta and McMaster would be my goto sources for barrels.

    edit: yep, still available.
    https://www.shapeways.com/product/FY...ionId=41639418

    edit edit: not universal barrel mount - designed for Crosman Defender auto-gun barrel/hop-up
    http://forums.trossenrobotics.com/sh...-design-thread
    https://www.thingiverse.com/thing:188424
    Last edited by tician; 10-22-2017 at 05:14 PM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: Go-to Airsoft weaponry solution?

    I think it's still available. I think I also marked the files as downloadable if you want them.
    They mate to a 1.5" tube for magazine, Pololu micro gearmotor for agitator, and the standard AEG form factor.
    They also mate to the hop-up and barrel from the $18 "defender" gun from Amazon. Scrap the gun, keep the barrel/hop-up...

    That being said, the gun will dry-fire every once in a while. The spring loaded flexible channel mechanism built by the R-Team folks seems more robust, albeit a bit more work to put together.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) what is the solution to this AVRDUDE problem
    By amir204 in forum Robotics General Discussion
    Replies: 0
    Last Post: 09-25-2015, 11:29 PM
  2. Bluetooth IO solution request
    By mSparks in forum Arbotix, Microcontrollers, Arduino
    Replies: 14
    Last Post: 03-23-2011, 01:09 PM
  3. Question(s) Small IP Camera Solution?
    By parallax in forum Sensors
    Replies: 6
    Last Post: 08-06-2010, 05:32 PM
  4. Looking for a cheap solution?
    By Borg in forum Mech Warfare
    Replies: 8
    Last Post: 06-09-2010, 10:55 AM
  5. A really clever charging solution
    By archcvd in forum Power
    Replies: 9
    Last Post: 09-22-2008, 04:31 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •