Results 1 to 4 of 4

Thread: Nokia in Bioloid?

  1. #1
    Join Date
    Jan 2007
    Location
    Near Robot Parts In The USA
    Posts
    232
    Rep Power
    47

    Nokia in Bioloid?

    I've seen the Bioloid Puppy videos with the Nokia head, and now I want one... Although I want a little more control over the robot so I'm thinking I'd use the USB to BUS board from HUV.

    The better Nokia N800 costs $250 USD, but the older 770 is on ebay for only $75 new!

    Does anyone know how hard to program a Nokia is, or even how to?

    Maybe I could call actions with VB on a webpage written on my XP computer, but would the Nokia's FireFox take that info and send it to the Bioloid correctly?

    The ideas are endless...
    Last edited by srobot; 02-04-2008 at 04:47 PM.
    Dell Studio XPS Desktop, Windows Vista, 12 GB RAM, 2x 500 GB SATA RAID0 HDD, Intel i7 2.66Ghz Quad Core (4 cores, 8 virtual cores). The power that's needed... plus some!

    RIBO Labs, Springing Robotic Development to a New Level

  2. #2
    Join Date
    Feb 2008
    Location
    Chicago, IL
    Posts
    9
    Rep Power
    38

    Re: Nokia in Bioloid?

    I doubted if USB to BUS board will work because that'll require the tablet to support USB host mode; but I think the tablet probably only work as a slave device. Best bet is still probably a bluetooth to serial device.

    To program the tablet, you'll need knowledge of C/C++ language, and to compile it & stuff, you need some knowledge in the SDK. More information can be found on maemo.org, and by the way, this software project might give you some idea about programming robot back end on tablet: http://garage.maemo.org/projects/robot/

  3. Re: Nokia in Bioloid?

    Actually, the N770, 800, and 810 all support USB host, although on the 770 (which I have) the usb port is unpowered, so you have to provide power to your USB devices from somewhere else. Once you solve the power issue, there is no reason you can't talk to my USB Bioloid bus board from a 770.

    As far as programming it goes, it runs Linux, so you will need to get up to speed on buildroot and gcc and all that crap...

    - Jon

  4. #4
    Join Date
    Feb 2008
    Location
    Chicago, IL
    Posts
    9
    Rep Power
    38

    Re: Nokia in Bioloid?

    Sorry I was wrong. According to this post: http://www.internettablettalk.com/fo...ad.php?t=13059. It did support USB host, and the OP actually succeeded in doing a USB to serial (with some mods of course).

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Molex is obsoleting the 3-pin straight connector used by the Bioloid
    By JonHylands in forum Humanoids, Walkers & Crawlers
    Replies: 8
    Last Post: 05-25-2010, 06:21 AM
  2. Contest Entry Bioloid Gripper
    By JonHylands in forum Project Showcase
    Replies: 12
    Last Post: 12-26-2008, 03:28 PM
  3. What to buy next Bioloid or Robonova.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 34
    Last Post: 03-05-2008, 05:49 PM
  4. Bioloid Tracked Base
    By JonHylands in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 09-12-2007, 10:35 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •