Results 1 to 3 of 3

Thread: Outdoor Robot Design - Wheels, Motor, Driver

  1. Outdoor Robot Design - Wheels, Motor, Driver

    Hi,

    I want to design and build an outdoor robot that can move across a flat lawn and carry a payload weighing about 10 – 15 Kg. Can you advise me regarding which parts might be suitable ?

    Here’s further information about the basic concept;-
    Overall weight about 15 Kg. Ground clearance at least 4 cm. Speed very slow (0.5 m/sec is OK). Payload platform area about 300 sq cm ( I expect to buy a sheet of thin aluminium and shape that ).
    Controlled by a Rashberry Pi or Arduino.

    I think what makes this robot concept different to many is the weight and the ground clearance.

    Could you advise me … what wheels, motors and motor driver would be suitable ?
    I think the motor torque will be important, given the weight and I can't find suitable sized wheels.

    Many thanks

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: Outdoor Robot Design - Wheels, Motor, Driver

    You are basically going to be looking for parts for a 30lbs class or 60lbs class combat robot or a FIRST robot, but requiring far less powerful motors and motor controllers since you do not need the speed to outmaneuver and overpower other robots. Banebots tends to be a very popular source for gearboxes, but AndyMark also produces some decent gearboxes and mechanical components. Plenty of hobbyking motors and motor controllers can be very useful when mated to a banebots gearbox, and many of their motor controllers can be reprogrammed with custom firmware.

    Robotmarketplace has a wide selection of wheels: http://www.robotmarketplace.com/prod...eels_main.html
    My last large rover project used $6 harborfreight 10-in. pneumatic tires and custom hubs, but it was a much heavier multipurpose outdoor robot dealing with rather steep hills throughout my yard.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: Outdoor Robot Design - Wheels, Motor, Driver

    I use 1/5th scale RC car wheels; they're about 7 inches (18 cm( around, so about 7 cm ground clearance depending on axle/motor mount.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Recommended motor driver to control stepper motor
    By Snoopy in forum Arbotix, Microcontrollers, Arduino
    Replies: 19
    Last Post: 03-27-2015, 08:06 PM
  2. Question(s) Newbie! Control a 12V DC Motor using 1061 Servo Controller and L298 Dual H-Bridge Motor Driver
    By dmar in forum Arbotix, Microcontrollers, Arduino
    Replies: 10
    Last Post: 09-05-2013, 03:32 PM
  3. Question(s) What sensors needed for outdoor robot?
    By Sergeant82d in forum Sensors
    Replies: 8
    Last Post: 10-13-2010, 02:05 AM
  4. Does this stepper motor need a driver?
    By Adman in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 03-20-2008, 11:26 AM
  5. Question(s) fixing Colson wheels on motor shaft
    By stefano.antonelli in forum Mechanics / Construction
    Replies: 6
    Last Post: 02-13-2008, 12:37 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •