Page 2 of 2 FirstFirst 12
Results 11 to 12 of 12

Thread: Open CM9.04 - How to connect to AX (or MX) servos?

  1. #11

    Re: Open CM9.04 - How to connect to AX (or MX) servos?

    If you're making your own board, you should make a board for a Teensy 3.2, not an OpenCM, in my opinion.
    (Well, that's what I've been doing :-)

  2. #12

    Re: Open CM9.04 - How to connect to AX (or MX) servos?

    Thanks Jwatte,

    As you probably know, I totally agree with you and what I have been doing as well.

    But trying to see how hard it would be to come up with a reasonably off the shelf setup that one could use to hypothetically build the Hexaod without using the Arbotix board as the controller. So trying to replace it's functionality.

    So if I were not going to build a complete custom board maybe something like:

    A) open CM9 board: Could use 904A board and solder in AX/MX connectors, but assume not... http://www.trossenrobotics.com/open-cm-904c
    B) XL to AX Servo cable - Have not found one available - but not hard to make..
    C) Use the Trossen Powered HUB - plug above cable into it. This gives you both the AX servo connectors and a power connection. May need second one for Hexapod http://www.trossenrobotics.com/6-port-ax-mx-power-hub

    D) XBee holder: Could us a stock Sparkfun one and then add on connector wires like https://www.amazon.com/Micro-Connect...t-ph+connector

    Or maybe a simple XBee board with JST ST type connector: Here is a quick and dirty version I setup in diptrace...
    Click image for larger version. 

Name:	XBEE-JST.jpg 
Views:	53 
Size:	39.8 KB 
ID:	7118
    Then use a cable to plug into the Serial2 connector on board. Maybe something like: https://www.adafruit.com/product/3568

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) How to connect 2 OpenCM9.04 wirelessly ?
    By Rouno in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 12-07-2017, 09:37 PM
  2. ROS os Connect to V-rep
    By curka in forum ROS - Robot Operating System
    Replies: 1
    Last Post: 09-30-2017, 05:47 PM
  3. Question(s) How can I connect 8 Flexiforce sensors?
    By Nina91 in forum Sensors
    Replies: 2
    Last Post: 01-04-2014, 04:22 PM
  4. How do you connect a NUC/Pi/Odroid to a PhantomX?
    By guruguhan in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 10-11-2013, 10:53 PM
  5. How to connect to FIRST CIM Motor (M4-R0062-12)?
    By scowby in forum Mechanics / Construction
    Replies: 4
    Last Post: 07-18-2011, 05:13 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •