Results 1 to 3 of 3

Thread: IR Filter (Ultrasonic too)

  1. #1
    Join Date
    Mar 2008
    Posts
    310
    Images
    49
    Rep Power
    51

    IR Filter (Ultrasonic too)

    I desire to build an electronics enclosure for my bot. Now, I would really like to make aesthetics somewhat a priority, if possible.

    To that end, I am looking for something to place in front of Sharp IR sensors, to hide the sensor behind. Ideally, whatever it is should be an opaque black in the visible spectrum to prevent someone seeing the sensor. The material should be stiff enough to prevent a mild impact, but thin enough to bend around a curve.

    Does anyone have any suggestions for what type of material I should be looking for? (and please, I am not interested in developed color film if that is what you are going to suggest)

    Also, the same question for ultrasonics (Daventech SRF series). Anyone know of a material or something that is black but doesn't really block the ultrasonic functioning?

    Thanks!

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    176

    Re: IR Filter (Ultrasonic too)

    Not very specific, but just to chime in, I'd do a search for ir bandpass filter

    One of the first promising links to turn up was: http://www.maxmax.com/aXNiteFilters.htm

    "
    X-Nite Infrared filters block all visible light letting only infrared light pass. Cutoff is 630nm, 665nm, 715nm, 780nm, 830nm, 850nm and 1000nm. These filters are for use on cameras that are infrared sensitive. Filters are constructed of optical precision ground and polished glass. They appear completely black to the human eye. If you hold the 830nm and 850nm filter up to a bright light, you will see the light filament faintly. If you hold the 1000nm filter to a bright light, the filter will appear completely opaque."

    Not cheap from this seller, but certainly that means someone else is. Shopping time! My favorite activity!

  3. #3

    Re: IR Filter (Ultrasonic too)

    For the ultrasonic sensors, you could maybe fashion a kind of speaker cover for them using sound transparent fabrics. I found some doing a quick Google search here: http://www.acousticalsolutions.com/p...rics/index.asp

    I'm not 100% sure if they are transparent to ultrasonic frequencies of sound, but I guess it's worth a look!
    It is far better to grasp the universe as it really is than to persist in delusion, however satisfying and reassuring. --Carl Sagan

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. IR Sensor with Phidget 8/8/8
    By lunarnexus in forum Sensors
    Replies: 4
    Last Post: 03-11-2008, 03:07 PM
  2. Question(s) Sharp IR sensor how to get information
    By BrandonG32 in forum Sensors
    Replies: 3
    Last Post: 02-08-2008, 10:04 AM
  3. Contest Entry Vex Robotics, Ultrasonic Bot 1.0, 2.0 and 3.0
    By srobot in forum Project Showcase
    Replies: 2
    Last Post: 08-29-2007, 04:18 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •