Results 1 to 3 of 3

Thread: Force Sensor equation from analog to lbs or force

  1. Force Sensor equation from analog to lbs or force

    Hi,
    I was wondering if there was an equation for the Force Sensor .2'' and .5'' that will allow me to get a meaningful value. I have the analog values that are coming out but I want to relate that to some type of force. Has there been equation already made out for these sensors? If so, can someone please push me in that direction. Thanks.

  2. #2

    Re: Force Sensor equation from analog to lbs or force

    If you take a look at the datasheet, there's a curve that correlates the resistance with force applied (well the weight of a mass in grams actually).

    http://www.trossenrobotics.com/image...FSR%20data.pdf

    You could take those points and have a calculator find an equation for you that would best fit the data then use the equation in your program. Since this equation takes resistance as a variable make sure you find out what resistance corresponds to what analog value so you know how to convert.

    Makes sense, right?
    It is far better to grasp the universe as it really is than to persist in delusion, however satisfying and reassuring. --Carl Sagan

  3. #3
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    174

    Re: Force Sensor equation from analog to lbs or force

    It may be a tad more complex. At a glance, the force v resistance graph is a power-law graph. So it's going to depend how accurate we need the fit to be. Ideally we'd turn to linear algebra here, and start looking to do regression analysis on the empiracle data. If we need to get a high level of precision, we'd probably start looking for work done that appears to fit our power law curve.

    I could feed it to MatLab later and see if it turns out a good fit quickly or if you'd just have to do regression to approximate every time.

    Another point to consider with force sensors is that you really need to do your own force testing in-situ, as the way you mount it, what it's mounted to, and what is surrounding it will greatly change your readings. Resistance isn't just electronic/electromechanical in this case, it's also purely mechanical.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Turning analog inputs into multi-switch digital inputs?
    By Clavis in forum Arbotix, Microcontrollers, Arduino
    Replies: 34
    Last Post: 01-09-2011, 11:42 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •