Results 1 to 2 of 2

Thread: Power Regulator Circuit Question for AX12a to XL-320

  1. #1
    floridianfisher Guest

    Power Regulator Circuit Question for AX12a to XL-320

    Hello,

    I have a bunch of AX-12As that I need to chain to XL-320s. I found this thread which says I can make a simple circuit with an SR05S7V2 but it is sold out and difficult to get in the US. Does anyone know of an alternative regulator that I can get or a existing product I can purchase to chain the servos together?

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: Power Regulator Circuit Question for AX12a to XL-320

    I made some small converter boards for AX12 to XL-320 with a pair of each connector type and the SR05S7V2, but never populated them since I never wound up using any XL-320 in my bots. I seem to recall other stating that the newer XL-320 firmware uses the DXL2.0 protocol, so cannot be used seamlessly with AX-12 servos (must create one sync_write packet in DXL1.x for AX servos on the buss and a second sync_write packet in DXL2.x for XL-320 servos on the buss).

    Digikey has currently an estimated ship date of 1/27 for the SR05S7V2, but still ~$6 each (https://www.digikey.com/product-deta...8-5-ND/4488627). Any cheap linear regulator in the TO-220 package/pinout would work just as well for a couple of XL-320 since they do not draw much current, although the 7V~7.5V range is not very common for fixed voltage regulators. The sequence of VIN/GND/VOUT is standard for the TO-220 linear 78xxx regulator, but which way the pins are arranged relative to the package can vary (some may have VIN/GND/VOUT as pins 1/2/3, or pins 3/2/1, respectively) which is usually not a big deal if you double check the polarity before wiring things up.

    A quick search of digikey produced several results in TO-220 package that should be in a pin-compatible with the SR05S7V2:
    STM's L78S75CV - https://www.digikey.com/product-deta...164-ND/1663449
    Rohm's BA17807T / BA78M07CP / BA07CC0T / BA7807CP / etc.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) AX12A power consumption
    By gmui in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 02-09-2017, 10:14 PM
  2. ax12a servos not getting power
    By deathwiz in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 04-13-2014, 06:22 PM
  3. Schematic question for LM138 voltage Regulator
    By wireframewolf in forum Power
    Replies: 6
    Last Post: 07-29-2012, 02:29 PM
  4. FlexiForce Drive Circuit: Power Supply
    By bioeng in forum Sensors
    Replies: 5
    Last Post: 10-28-2009, 02:28 AM
  5. Replies: 6
    Last Post: 09-28-2007, 07:38 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •