Results 1 to 2 of 2

Thread: Can I replace ARbotix with Arduino Mega 2560?

  1. Can I replace ARbotix with Arduino Mega 2560?

    This is my second ARbotix board which works fine for some days then it will become impossible to upload the code because of the content mismatch error. I just want to get rid of Arbotix-M. Can I replace it with ARduino MEga 2560?

    I'm making the PhantomR
    http://www.trossenrobotics.com/p/pha...robot-arm.aspx

    Your helpful suggestions will be appreciated.

  2. #2

    Re: Can I replace ARbotix with Arduino Mega 2560?

    The answer is yes... With certain caveats.

    That is their default libraries are hard coded to bypass the Serial object... I have a version of the library up at github...
    https://github.com/kurte/bioloidserial which is setup to handle on different Serial objects, like Serial1 on Arduino mega.

    You then need to wire it up to work half duplex... I have done this in the past connecting up the RX/TX pins of one of the Serial ports to each other and to the Data pin of an Bioloid connector and also needed to connect up a common ground...

    Note this does not provide the Arduino any protection from anything going wrong on the TTL data line. The AX12 manual shows their prefered hookup.... But I never had problems with hurting an Arduino...

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Setting up Arduino Mega 2560 with RC input control with modified Phantom X
    By powerover in forum Arbotix, Microcontrollers, Arduino
    Replies: 39
    Last Post: 12-27-2016, 05:07 PM
  2. Question(s) Can Arbotix Pro easily replace the Arbotix-M in my robot?
    By NSz in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 05-23-2016, 02:12 PM
  3. Arduino Mega 2560 and Serial Comunication issues
    By DVS in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 07-10-2013, 02:31 PM
  4. Arduino Mega 2560 and AX12A servos
    By DVS in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 07-08-2013, 04:26 PM
  5. Arduino Mega 2560 and AX12A servos
    By DVS in forum Sensors
    Replies: 1
    Last Post: 07-08-2013, 04:09 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •