Results 1 to 3 of 3

Thread: Well my 2nd post with a question about phone lines

  1. Well my 2nd post with a question about phone lines

    I am a new person here, but here is my problem.
    I am modifying a wireless phone set. A base station that is attached to my computer modem using a phone line wire, and the wireless part aka the headset, is going to be attached to the bot. I am planning to use serout and serin through the wireless connection, but I am having a difficult time with the wiring. I have found the actual wireless part of both units which is covered by metal shielding, probably against and feedback or noise, but only one has markings such as which of the wires are tx, rfi-power, etc, the other does not. And even with the markings it is difficult to conclude which does what exactly. Any help would be nice :P. I am planing to run some script on my pc to send data to and fro the bot using the wireless component of the head set and base station. The bot's brains are going to be a bs2. Pics of this can be seen here.

    The headset:
    http://i121.photobucket.com/albums/o...z/P1020636.jpg
    http://i121.photobucket.com/albums/o...z/P1020635.jpg

    The base station wireless uncovered:
    http://i121.photobucket.com/albums/o...z/P1020634.jpg
    http://i121.photobucket.com/albums/o...z/P1020633.jpg
    http://i121.photobucket.com/albums/o...z/P1020631.jpg

    Much thanks for reading and hopefully helping me out.

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    178

    Re: Well my 2nd post with a question about phone lines

    If I understand your needs correctly, you're going to need to modulate and demodulate the signal to get it into the digital domain. Interestingly enough, that's what "MODEM" stands for - Modulator DeModulator.

  3. Re: Well my 2nd post with a question about phone lines

    You may want to check out some off-the-shelf Bluetooth modems instead. The Blue SMiRF transceivers act as wireless serial bridges. They're well-documented and relatively idiot-proof.

    http://www.trossenrobotics.com/spark...rf-silver.aspx

    I mean, I don't want to talk you out of using the cordless phone, because you will save yourself a lot of money that way, but you may also end up pulling out a lot of hair.
    New to the TR Community? Feel free to introduce yourself and show off your projects!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •