Results 1 to 2 of 2

Thread: Arbotix serial ports

  1. #1

    Arbotix serial ports

    Hello everyone,


    I open this forum because I need to know if I can use some of the digital pins of the arbotix as another serial port, since I need to have two different ways to communicate with two computers, a serial port to move some engines and another port to make a graphical interface among them.


    Thank you!!


    Urko.

  2. #2

    Re: Arbotix serial ports

    The Arbotix-M has two serial ports:
    The first Serial port is typically either the XBee or the FTDI cable (both use same pins).
    The Second Serial port is the one that is actually used to drive the servos.

    The only option beyond that is to use something like the SoftwareSerial library, to create a serial port. But there are limitations on how well that works.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Serial Transmission being interrupted by Serial Receiver [Arbotix + Dynamixel AX-12 + LIDAR Lite]
    By rishflab in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 04-14-2015, 06:05 PM
  2. Serial communication between Arduino and Arbotix
    By dburongarcia in forum Arbotix, Microcontrollers, Arduino
    Replies: 17
    Last Post: 03-09-2014, 01:44 PM
  3. Is there a fix for the miss-aligned analog ports on the Arbotix-m
    By crchisholm in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 02-10-2014, 08:33 AM
  4. Question(s) Arbotix and Arduino Software Serial Library
    By Jules in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 06-21-2012, 11:19 AM
  5. Question(s) Help Arbotix Robocontroler Hobby Servo ports
    By tiburcio in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 03-10-2011, 12:10 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •