Results 1 to 10 of 10

Thread: Writing code on a Mac...reccomendations?

  1. Writing code on a Mac...reccomendations?

    Hello everyone-

    I am brand new to both these forums and programming and detailed electronics in general. I did some basic wiring for my high school's robotics team, but nothing that really got down to the sensor level, and I didn't even touch the code (much to my now recognized chagrin).

    My friend has offered to let me borrow some of his phidgets, but I have no way to write code. Does anyone here use a mac to write their code? If so, what do you use? Free is always better, and in my case may be the only option.

    Any other pieces of advice would be gladly welcomed.

    Thanks!
    Adam

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    181

    Re: Writing code on a Mac...reccomendations?

    Here: http://www.phidgets.com/downloads.php?os_id=2 is a list of the environments supported on OSX. Each have descriptive links. Does that help?

    BTW: Welcome to the TRC!

  3. Re: Writing code on a Mac...reccomendations?

    That is exactly the page I was looking for! Thank you so much!

  4. #4
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    102

    Re: Writing code on a Mac...reccomendations?

    I use software called Max/msp...definately not free...but you get 30 days to figure it out. There is a free version called pure data or PD. Phidgets has a whole library of objects for it.

    DB

  5. Re: Writing code on a Mac...reccomendations?

    Already lost, not a good sign...
    What do I open to start writing code? I installed the first part, and it works as far as I am concerned, but do I need to have a phidget connected in order to edit/write the code associated with it?

  6. #6
    Join Date
    Mar 2008
    Posts
    310
    Images
    49
    Rep Power
    56

    Re: Writing code on a Mac...reccomendations?

    Xcode (free from developer.apple.com or on your OS CDs) is the defacto IDE for Macs I believe. I can't wait to get back to having a Mac as my primary system*.

    *Right now I use Windows on a custom built box, due to price, and it runs Autocad. Eventually I will get a nice Intel Mac, and then be able to use Parallels and all that My current Macs are a G4 and G5.
    Last edited by Sienna; 06-13-2008 at 07:22 AM. Reason: Wrong processor cores... ooops

  7. #7
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    113

    Re: Writing code on a Mac...reccomendations?

    hey DB! Isn't your tutorial on MAX/MSP with Phidgets using a Mac?

    http://forums.trossenrobotics.com/showthread.php?t=1845

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  8. #8

    Re: Writing code on a Mac...reccomendations?

    Hey Ninja,

    I use a mac for day to day, but I do all my c coding in linux. I suggest, if your serious about developing in something other can cocoa/objective c, to get a VM and run a flavor of linux; debian, ubuntu, FC, etc.

    You'll be able to get all the latest tools, libraries via the simple apt-get package management system. Yes, I realize osx has fink and darwin ports, but I feel both those PMs are not as good as what comes on linux distros.

    Also, I think you'll be able to get more help if your using a *nix. There isn't as much robotic development happening on osx as there is on xp/*nix.

    Just my .02$.

    - sk

  9. #9
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    102

    Re: Writing code on a Mac...reccomendations?

    Hey,

    If you do run Linux, you can run Pure Data. Its the free version of the MAX/MSP language that I program in. There are a wide variety of libraries people have written for Pure Data, and it is constantly evolving.

    You can also spring for MAX...then I wouldn't be all alone.

    DB

  10. #10
    Join Date
    Jun 2008
    Location
    San Francisco
    Posts
    33
    Rep Power
    42

    Re: Writing code on a Mac...reccomendations?

    a bit off topic, but I use either macs or FreeBSD for my personal projects. I tend to code in either emacs for portability (ie, I can work on it wherever, save my stuff in subversion, have the same window up at home or at work, etc). But I've been using TextMate for OS X to write my ruby code, and it's quite the dream. Three or 4 keypress shortcuts to set up data structures, errors during runtime link me back to the code, etc.

    That said, for vision stuff (and at work) I go with linux. Usually debian.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Apple's Designer Scared!
    By srobot in forum Off Topic
    Replies: 8
    Last Post: 03-14-2008, 01:08 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •