Page 2 of 2 FirstFirst 12
Results 11 to 12 of 12

Thread: Issues connecting Odroid XU4 to Arbotix Pro

  1. #11
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,240
    Images
    27
    Rep Power
    271

    Re: Issues connecting Odroid XU4 to Arbotix Pro

    With servos respond inconsistently, it is usually caused by a power supply and/or cabling issue. The only time I've had an issue with a CM-730/Arbotix-Pro was occasional refusal to even appear as a USB device when it was used in a DARwIn-OP, but that was almost certainly caused by the fit-pc2i in that DARwIn-OP since the issue occurred on only one bot but with two different CM-730 and three different usb cables.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  2. #12

    Re: Issues connecting Odroid XU4 to Arbotix Pro

    Agree with Tician,

    I would also check to see if it is always consistently missing the same item, I believe in the case you showed was #10. Or is it semi random.

    Again if it were me, I would try to use a Logic Analyzer to see if the servo is not responding at all or if it maybe responded but data was corrupted, or data was slow and the the code had already started to try to send for the next servo id...

    If it was always missing one or more, I would start looking to see if one or more servos reset to ID#1, but does not sound like it here

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Multiple issues, Arbotix-M, pinxher/widowx + ROS
    By noreng in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 04-03-2017, 04:58 PM
  2. Question(s) MX/AX servo arm - trouble connecting via ArbotiX
    By a_saf in forum Interbotix Robotic Arms
    Replies: 20
    Last Post: 06-17-2016, 09:22 AM
  3. Problems with Arbotix Pro connecting to servos
    By Weebo in forum HR-OS1 Development and Discussion
    Replies: 1
    Last Post: 10-06-2015, 05:58 PM
  4. Question(s) Connecting ultrasound sensor to arbotix
    By vassilissa in forum Sensors
    Replies: 1
    Last Post: 04-15-2014, 03:33 AM
  5. Issues with Arbotix Programming- avrdude: stk500_getsync() error
    By Nitro in forum Software and Programming
    Replies: 4
    Last Post: 12-11-2012, 01:41 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •