Results 1 to 2 of 2

Thread: Actuators blinking RED upon boot

  1. #1
    squared9 Guest

    Question Actuators blinking RED upon boot

    Hi,

    I haven't used HR-OS1 for a few months and once I got back to it, when I turn on the power most of actuators blink RED and robot no longer fixes its position. I am wondering how to debug what is going on? I guess by leaving it without any movement for a while something has changed in actuators or maybe some contacts got dirty. I also made sure LiPo was fully charged.

    How would you try to diagnose the issue?

    Thanks!

  2. #2

    Re: Actuators blinking RED upon boot

    Sorry,

    Not sure what you are saying.

    If you say when you turn the power on the servos blink once? If so that is normal for these servos.

    As for not holding position. Warning it has been a couple/few years since I touched mine, so I don't remember much...

    Might help if there was additional information, like what processor are you using? Edison, RPI, or other.
    What program you ran to get it to hold it's position and if it showed any output information.

    You might also want to run the dxl_monitor program and see if it can talk to your servos...

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. SSC-32U LED A keeps blinking
    By powerover in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 10-14-2017, 02:04 PM
  2. Blinking Red Light AX-12A
    By deathwiz in forum DYNAMIXEL & Robot Actuators
    Replies: 11
    Last Post: 12-03-2014, 12:21 PM
  3. Bioloid CM 530 Boot Loader
    By Ray in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 08-25-2014, 03:49 PM
  4. Question(s) Roboard, Linux, boot times?
    By RogueWarrior65 in forum Robot Computers
    Replies: 0
    Last Post: 07-24-2009, 02:39 PM
  5. Question(s) PX5000EG boot-up malfunction
    By mdurna in forum Robot Computers
    Replies: 6
    Last Post: 02-15-2009, 12:28 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •