Results 1 to 5 of 5

Thread: Motor model for XM430-W350-R

  1. Motor model for XM430-W350-R

    Hello all,

    Hoes anyone figured out the motor contained in the XM40-W350-R? Is it a Maxon RE-max series motor like the MX-28? (I am trying to build a mathematical motor model and i look for the motor parameters)

    Best regards

  2. #2

    Re: Motor model for XM430-W350-R

    The XM series uses some cheaper motor. The XH series uses Maxxon motors, hence the higher cost (and, unfortunately, lower rated performance!)

  3. Re: Motor model for XM430-W350-R

    Thank you for your response! Do you know if it is a brushed or brushless motor?

  4. #4

    Re: Motor model for XM430-W350-R

    I believe it is a coreless brushed motor.

  5. Re: Motor model for XM430-W350-R

    To answer myself, per my calculations/experiments:

    R=4.6
    Kt=0.0046
    Kb=0.0069
    J=3.42e-7
    K_damping=1.35e-07
    L=69.6e-3

    Values are in S.I. Take them with a grain of salt.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Cannot connect to Dynamixel XM430-W210-T by USB2Dynamixel adapter
    By robomaniacpl in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 02-14-2018, 10:44 PM
  2. gearbox 3d model
    By sthmck in forum Mech Warfare
    Replies: 1
    Last Post: 12-11-2014, 08:54 PM
  3. 3D Model Thread?
    By YoMarchYo in forum Mech Warfare
    Replies: 0
    Last Post: 04-07-2013, 02:40 AM
  4. CAD Model of Phidgets
    By cmmguy in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 04-23-2008, 03:56 PM
  5. Robotic Model Building
    By Rick Badman in forum Robotics General Discussion
    Replies: 2
    Last Post: 08-27-2007, 10:29 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •