Page 1 of 2 12 LastLast
Results 1 to 10 of 17

Thread: 2018 Robogames Mech Target Plates/Transponder

  1. #1
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    225
    Rep Power
    25

    2018 Robogames Mech Target Plates/Transponder

    Click image for larger version. 

Name:	RTEAM.JPG 
Views:	120 
Size:	11.7 KB 
ID:	7184

    We've made a few changes to the target plates for 2018. For the most part, these changes will be transparent to the end Mech user.

    As in 2017, R-Team will be providing the target plates to each competitor just prior to the match start. In addition, we will also be providing the transponder as well. I repeat, for 2018 Robogames, competitors will NOT need to provide a transponder. The transponder is integrated into the back target plate. The mounting method, of the target plates to the Mech will be identical to 2017.

    Info on how to mount the target plates can be found here:
    http://forums.trossenrobotics.com/sh...-Target-Plates
    https://github.com/ghengisdhon/rbots/blob/master/Target%20Plates%202017/2017%20Robogames%20Target%20Plates.pdf

    The major difference (for Mech Builders) to the 2018 plates from the 2017 plates is that they now use 4-pin Dynamixel connectors. We highly recommend that competitors integrate the harness/connectors through their mech. Basically, you need a harness from each target plate location on your mech, to the back target plate location on your mech. (We will have limited loaners available.)

    The 4-Pin Dynamixel connectors can be bought from Trossen here:
    http://www.trossenrobotics.com/store...e-10-Pack.aspx
    http://www.trossenrobotics.com/store...e-10-Pack.aspx
    http://www.trossenrobotics.com/store...e-10-Pack.aspx
    http://www.trossenrobotics.com/store...e-10-Pack.aspx
    http://www.trossenrobotics.com/store...e-10-Pack.aspx

    Hope this isn't to confusing... if you have questions, let me know and I'll try to clarify.

  2. #2

    Re: 2018 Robogames Mech Target Plates/Transponder

    Is there some kind of interactivity between the scoring system and the 'mech, such as telling the 'mech where it's hit and what the score is?
    Or, barring that, is the network protocol going to be finally robust and easy to use? :-D

    (Not that I'm building a new mech or anything. I don't have time for that. Just checking.)

  3. #3
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    225
    Rep Power
    25

    Re: 2018 Robogames Mech Target Plates/Transponder

    Quote Originally Posted by jwatte View Post
    Is there some kind of interactivity between the scoring system and the 'mech, such as telling the 'mech where it's hit and what the score is?
    Or, barring that, is the network protocol going to be finally robust and easy to use? :-D

    (Not that I'm building a new mech or anything. I don't have time for that. Just checking.)
    Click image for larger version. 

Name:	RTEAM.JPG 
Views:	57 
Size:	11.7 KB 
ID:	7365

    Such privileged information only goes to those who are ACTUALLY building a mech! Honestly though, there used to be a pin on the transponder board that indicated the hit & location. We've respun the boards a few times and have been trying to minimize the board foot print, so I'll have to check with Artans and see if it has survived all the revisions.

  4. #4

    Re: 2018 Robogames Mech Target Plates/Transponder

    In the best of worlds, that pin wouldn't use the hundreds-of-milliseconds pulse protocol, but instead send a UART byte at 115,200 bps or something like that ... A value something like:

    Code:
    (0x80 if counted, 0x00 if not counted) | ((panelid & 3) << 5) | (remaining hitpoints)
    And if you're out of serial capability, doing the same with a soft-serial at 9600 bps would still be alright :-)

  5. #5

    Re: 2018 Robogames Mech Target Plates/Transponder

    Quote Originally Posted by jwatte View Post
    In the best of worlds, that pin wouldn't use the hundreds-of-milliseconds pulse protocol, but instead send a UART byte at 115,200 bps or something like that ... A value something like:

    Code:
    (0x80 if counted, 0x00 if not counted) | ((panelid & 3) << 5) | (remaining hitpoints)
    And if you're out of serial capability, doing the same with a soft-serial at 9600 bps would still be alright :-)
    To detect hits, it's still the legacy pulse. The pulse will be 50-200 ms based on which plate was hit. Unfortunately right now the pulse only happens when it scores a hit, so it doesn't tell you when you're getting hit and it doesn't count. The transponder works off 3.3V now using a 1s LiPo. The signal with the pulse is open collector now.

    If we redo it, I'll consider implementing software serial.
    Last edited by artans; 12-06-2018 at 10:12 AM. Reason: clarification

  6. #6

    Re: 2018 Robogames Mech Target Plates/Transponder

    Thanks for the info!

  7. #7
    Join Date
    Jun 2011
    Location
    USA
    Posts
    533
    Images
    107
    Rep Power
    39

    Re: 2018 Robogames Mech Target Plates/Transponder

    Assuming we're using this same setup next month, can we get dimensions of where the 4pin connector is located on each score panel? I want to make sure I have clearance for the cable that will plug in... (better yet, potentially, did we consider using right-angle dynamixel connectors, rather than perpendicular to the target panel?

  8. #8
    Join Date
    Feb 2012
    Location
    Tucson, Arizona
    Posts
    144
    Rep Power
    27

    Re: 2018 Robogames Mech Target Plates/Transponder

    They are right angle connectors pointed down. A little above horizontal center. From the backside right of vertical center. I'll get some measurements and a picture to post tonight. No one has had an interference problem with them so far.

  9. #9

    Re: 2018 Robogames Mech Target Plates/Transponder

    If it's like the previous ones, it's centered horizontally and about an inch down vertically. That's my current assumption until I'm proven differently!

  10. #10
    Join Date
    Feb 2012
    Location
    Tucson, Arizona
    Posts
    144
    Rep Power
    27

    Re: 2018 Robogames Mech Target Plates/Transponder

    I was a little wrong in the previous description. This is the latest rev C plate from late 2017. Still current. Target plate is 3.5 x 3.5 inches with a Velcro strip down each vertical side. The connector is a right angle 4 pin male facing down. The center of the connector body is about 1.5" from the bottom and about 1.25" from the side. The mating female connector plugs in from bottom side of the male connector.

    Click image for larger version. 

Name:	DSC02068.jpg 
Views:	18 
Size:	93.7 KB 
ID:	7501 Click image for larger version. 

Name:	DSC02069.jpg 
Views:	16 
Size:	86.2 KB 
ID:	7502 Click image for larger version. 

Name:	DSC02070.jpg 
Views:	15 
Size:	92.9 KB 
ID:	7503 Click image for larger version. 

Name:	DSC02067.jpg 
Views:	15 
Size:	96.0 KB 
ID:	7504
    Last edited by giantflaw; 3 Weeks Ago at 11:45 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Robogames 2018 Mech Warfare Ruleset
    By giantflaw in forum Mech Warfare
    Replies: 8
    Last Post: 06-06-2018, 11:53 AM
  2. 2018 Robogames Mech Warfare Qualifying
    By GhengisDhon in forum Mech Warfare
    Replies: 17
    Last Post: 04-25-2018, 11:22 AM
  3. Robogames 2018 Ideas and Suggestions
    By GhengisDhon in forum Mech Warfare
    Replies: 24
    Last Post: 02-05-2018, 08:57 PM
  4. Mech Warfare Scoring Transponder 2017
    By artans in forum Mech Warfare
    Replies: 33
    Last Post: 04-16-2017, 12:57 AM
  5. 2017 Mech Target Plates
    By GhengisDhon in forum Mech Warfare
    Replies: 23
    Last Post: 03-27-2017, 09:32 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •