Page 2 of 2 FirstFirst 12
Results 11 to 16 of 16

Thread: 2018 Robogames Mech Target Plates/Transponder

  1. #11
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    42

    Re: 2018 Robogames Mech Target Plates/Transponder

    Thanks for the pictures! Am I correct in understanding that the back panel will have 3 (or 4?) connectors, plus an integrated 1S battery (I don't recall where I read that).

  2. #12
    Join Date
    Feb 2012
    Location
    Tucson, Arizona
    Posts
    164
    Rep Power
    29

    Re: 2018 Robogames Mech Target Plates/Transponder

    Yes, it's about 1 inch thick and meant to go in the back of the robot but it could go anywhere. You feed 3 small wire harnesses through the robot to connect the 3 regular plates to the one in the back. You can see the 3 open male pin connectors below. There is a built in battery, transponder, radio, impact sensor and switch. It Velcros on like the other plates. You can provide your own wire harness or we will bring plenty of extras of varying length for people to borrow along with the plates.

    Click image for larger version. 

Name:	DSC02074.jpg 
Views:	85 
Size:	112.1 KB 
ID:	7505 Click image for larger version. 

Name:	DSC02073.jpg 
Views:	83 
Size:	99.8 KB 
ID:	7506Click image for larger version. 

Name:	DSC02075.jpg 
Views:	80 
Size:	91.1 KB 
ID:	7507Click image for larger version. 

Name:	DSC02072.jpg 
Views:	82 
Size:	96.5 KB 
ID:	7508

  3. #13
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    42

    Re: 2018 Robogames Mech Target Plates/Transponder

    Awesome, thanks for the pics!

  4. #14
    Join Date
    Sep 2010
    Posts
    206
    Images
    16
    Rep Power
    39

    Re: 2018 Robogames Mech Target Plates/Transponder

    I noticed there was a 2"-18" limit for the panel mounting height, what about 1" height off the ground? I may have already designed it to like 1.5" I think...

  5. #15
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    252
    Rep Power
    27

    Re: 2018 Robogames Mech Target Plates/Transponder

    We've had discussions about that rule in the past as well. It was a legacy rule and we're not sure what the rationale behind it was. The way I see it if your under 2" of the ground its potentially more of a disadvantage than an advantage. More likely to catch ricocheting BBs as well as bumping into ground clutter.

    We'll waive the rule if you come under 2".

  6. #16
    Join Date
    Feb 2012
    Location
    Tucson, Arizona
    Posts
    164
    Rep Power
    29

    Re: 2018 Robogames Mech Target Plates/Transponder

    I just re-read the 2018 rule set. The 2" was taken out as far as I can see. Section VII paragraph 5 at the Robogames 2018 site.

    5. Target plates must be reasonably and FIRMLY mounted on a Mech, with their entire face located less than 22” off the ground, and not obscured by any limbs. Plates should be mounted on a flat, vertical surface, using two strips of 3.5” length velcro, so that the target plate is perpendicular to the ground.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Robogames 2018 Mech Warfare Ruleset
    By giantflaw in forum Mech Warfare
    Replies: 8
    Last Post: 06-06-2018, 11:53 AM
  2. 2018 Robogames Mech Warfare Qualifying
    By GhengisDhon in forum Mech Warfare
    Replies: 17
    Last Post: 04-25-2018, 11:22 AM
  3. Robogames 2018 Ideas and Suggestions
    By GhengisDhon in forum Mech Warfare
    Replies: 24
    Last Post: 02-05-2018, 08:57 PM
  4. Mech Warfare Scoring Transponder 2017
    By artans in forum Mech Warfare
    Replies: 33
    Last Post: 04-16-2017, 12:57 AM
  5. 2017 Mech Target Plates
    By GhengisDhon in forum Mech Warfare
    Replies: 23
    Last Post: 03-27-2017, 09:32 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •