Results 1 to 6 of 6

Thread: ArbotiX-M / Dynamanager function error

  1. ArbotiX-M / Dynamanager function error

    Hello Everyone,

    I am new to the forum and I am quite new to the world of electronics, I am probably less experienced than the majority of you so please be patient
    I am trying to upgrade my skills quickly and for my new project I am using Dynamixel AX-12Amotors. I am trying to do my best to learn fast!


    I am facing few issues at the moment and I would really appreciate if anyone could give me some help!


    First problem I am having is with Dynamanager. I followed all the steps on the trossen pages and downloaded ControlP5 Library and Dynamanager code. When I run the processing file it gives all sorts of errors like: the function valueLabel() does not exist. Then I managed to fix it at some point but the it said style does not exist and so on (line 188).
    I checked multiple times and I copied the libraries in the processing folder so that should be fine.

    Does any of you faced same problems? Is there any tutorial that expalin more in depth how to run dynamanager?

    Thanks in advance !!


  2. #2

    Re: ArbotiX-M / Dynamanager function error

    How do you run the processing file? It sounds like you're not running it in the right processing environment?

  3. Re: ArbotiX-M / Dynamanager function error

    Thanks a lot jwatte for your reply,I didn't have the batch file in the version I downloade and I was running the source code. Now i re-downloaded the pakage and it worked!!

  4. Re: ArbotiX-M / Dynamanager function error

    Quote Originally Posted by jwatte View Post
    How do you run the processing file? It sounds like you're not running it in the right processing environment?
    I am new to this as well, and having basically the same problem.

    I just purchased the PhantomX Robot Turret kit and am working though the setup outlined at:




    I got past steps 5 and 6 ("Blink" and "Control a DYNAMIXEL Servo").

    The first time through, I overlooked the next link under "Next: Set DYNAMIXEL IDs" and instead went back to the previous page.

    On the PhantomX Turret page, there is a different section where I left off entitled "Setting Your DYNAMIXEL IDs", which leads me to this page about setting up Dynamanager:




    I uploaded the ROS.ino sketch to the Arbotix-M, and then downloaded and ran the .BAT in the paretn folder of dynaManager13_win_64_java. I interpret this to be a compiled version of DynaManager. The UI loads, but as soon as I send a command an error dump occurs:
    #
    # A fatal error has been detected by the Java Runtime Environment:
    #
    # EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x000000007110b5db, pid=11780, tid=0x00000000000004cc
    #
    # JRE version: Java(TM) SE Runtime Environment (8.0_261-b12) (build 1.8.0_261-b12)
    # Java VM: Java HotSpot(TM) 64-Bit Server VM (25.261-b12 mixed mode windows-amd64 compressed oops)
    # Problematic frame:
    # C [jSSC-2.8.dll+0xb5db]
    #
    # Failed to write core dump. Minidumps are not enabled by default on client versions of Windows

    So, I downloaded and installed Processing, and I placed the ControlP5 library where recommended. Then, in Processing, I selected File > Open > dynaManager.pde and selected Run. I see the same error mentioned, " The function "valueLabel()" does not exist" at lines 188 and 228. I also see "The class "ListBoxItem" does not exist" at line 360 and "The value of the local variable "curServoid" is not used" at line 384.

    As I was writing this, I figured out that there was a link at the bottom of the page:




    entitled "Next: Set DYNAMIXEL IDs", and this takes me to "Setting DYNAMIXEL AX and MX Series Firmware, ID, and BAUD with ROBOPLUS 1.0". I downloaded and installed ROBOPLUS 1.0, set the COM port to COM21, and tried searching for the one connected Dynamixel, but it did not find the device.

    So, I am stuck. Any assistance would be appreciated.


  5. Re: ArbotiX-M / Dynamanager function error

    Quote Originally Posted by jwatte View Post
    How do you run the processing file? It sounds like you're not running it in the right processing environment?
    I am new to this as well, and having basically the same problem.

    I just purchased the PhantomX Robot Turret kit and am working though the setup outlined at:




    I got past steps 5 and 6 ("Blink" and "Control a DYNAMIXEL Servo").

    The first time through, I overlooked the next link under "Next: Set DYNAMIXEL IDs" and instead went back to the previous page.

    On the PhantomX Turret page, there is a different section where I left off entitled "Setting Your DYNAMIXEL IDs", which leads me to this page about setting up Dynamanager:




    I uploaded the ROS.ino sketch to the Arbotix-M, and then downloaded and ran the .BAT in the paretn folder of dynaManager13_win_64_java. I interpret this to be a compiled version of DynaManager. The UI loads, but as soon as I send a command an error dump occurs:
    #
    # A fatal error has been detected by the Java Runtime Environment:
    #
    # EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x000000007110b5db, pid=11780, tid=0x00000000000004cc
    #
    # JRE version: Java(TM) SE Runtime Environment (8.0_261-b12) (build 1.8.0_261-b12)
    # Java VM: Java HotSpot(TM) 64-Bit Server VM (25.261-b12 mixed mode windows-amd64 compressed oops)
    # Problematic frame:
    # C [jSSC-2.8.dll+0xb5db]
    #
    # Failed to write core dump. Minidumps are not enabled by default on client versions of Windows

    So, I downloaded and installed Processing, and I placed the ControlP5 library where recommended. Then, in Processing, I selected File > Open > dynaManager.pde and selected Run. I see the same error mentioned, " The function "valueLabel()" does not exist" at lines 188 and 228. I also see "The class "ListBoxItem" does not exist" at line 360 and "The value of the local variable "curServoid" is not used" at line 384.

    As I was writing this, I figured out that there was a link at the bottom of the page:




    entitled "Next: Set DYNAMIXEL IDs", and this takes me to "Setting DYNAMIXEL AX and MX Series Firmware, ID, and BAUD with ROBOPLUS 1.0". I downloaded and installed ROBOPLUS 1.0, set the COM port to COM21, and tried searching for the one connected Dynamixel, but it did not find the device.

    So, I am stuck. Any assistance would be appreciated.


  6. Re: ArbotiX-M / Dynamanager function error

    Quote Originally Posted by jwatte View Post
    How do you run the processing file? It sounds like you're not running it in the right processing environment?
    I am new to this as well, and having basically the same problem.

    I just purchased the PhantomX Robot Turret kit and am working though the setup outlined at:




    I got past steps 5 and 6 ("Blink" and "Control a DYNAMIXEL Servo").

    The first time through, I overlooked the next link under "Next: Set DYNAMIXEL IDs" and instead went back to the previous page.

    On the PhantomX Turret page, there is a different section where I left off entitled "Setting Your DYNAMIXEL IDs", which leads me to this page about setting up Dynamanager:




    I uploaded the ROS.ino sketch to the Arbotix-M, and then downloaded and ran the .BAT in the paretn folder of dynaManager13_win_64_java. I interpret this to be a compiled version of DynaManager. The UI loads, but as soon as I send a command an error dump occurs:
    #
    # A fatal error has been detected by the Java Runtime Environment:
    #
    # EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x000000007110b5db, pid=11780, tid=0x00000000000004cc
    #
    # JRE version: Java(TM) SE Runtime Environment (8.0_261-b12) (build 1.8.0_261-b12)
    # Java VM: Java HotSpot(TM) 64-Bit Server VM (25.261-b12 mixed mode windows-amd64 compressed oops)
    # Problematic frame:
    # C [jSSC-2.8.dll+0xb5db]
    #
    # Failed to write core dump. Minidumps are not enabled by default on client versions of Windows

    So, I downloaded and installed Processing, and I placed the ControlP5 library where recommended. Then, in Processing, I selected File > Open > dynaManager.pde and selected Run. I see the same error mentioned, " The function "valueLabel()" does not exist" at lines 188 and 228. I also see "The class "ListBoxItem" does not exist" at line 360 and "The value of the local variable "curServoid" is not used" at line 384.

    As I was writing this, I figured out that there was a link at the bottom of the page:




    entitled "Next: Set DYNAMIXEL IDs", and this takes me to "Setting DYNAMIXEL AX and MX Series Firmware, ID, and BAUD with ROBOPLUS 1.0". I downloaded and installed ROBOPLUS 1.0, set the COM port to COM21, and tried searching for the one connected Dynamixel, but it did not find the device.

    So, I am stuck. Any assistance would be appreciated.


Thread Information

Users Browsing this Thread

There are currently 3 users browsing this thread. (0 members and 3 guests)

Similar Threads

  1. Question(s) Error uploading arduino program to arbotix card
    By urko_18 in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 11-21-2017, 09:53 AM
  2. Question(s) ArbotiX avrdude error
    By arbotix in forum Software and Programming
    Replies: 4
    Last Post: 08-19-2017, 03:49 AM
  3. stk500 Error with new Arbotix-M board
    By BakaPixel in forum Arbotix, Microcontrollers, Arduino
    Replies: 10
    Last Post: 03-28-2017, 02:34 AM
  4. Arbotix m and Dynamanager on mac
    By wthierry in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 08-12-2014, 08:15 PM
  5. Issues with Arbotix Programming- avrdude: stk500_getsync() error
    By Nitro in forum Software and Programming
    Replies: 4
    Last Post: 12-11-2012, 02:41 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •