Results 1 to 4 of 4

Thread: Dynamixel 2.0 feature!

  1. #1

    Dynamixel 2.0 feature!

    Spotted this new feature in the MX-64 firmware:


  2. #2

    Re: Dynamixel 2.0 feature!

    Nice catch, It is also in the new XL series Servos:
    http://support.robotis.com/en/produc...htm#bookmark43
    After firmware version 38...

  3. #3
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    92

    Re: Dynamixel 2.0 feature!

    Ok stupid question, what is Bus Watchdog.

  4. #4

    Re: Dynamixel 2.0 feature!

    According to the bookmark above:
    Bus Watchdog (98, Available after Firmware version 38)
    Bus Watchdog (98) is a safety device (Fail-safe) that stops the Dynamixel if the communication between the controller and Dynamixel communication (RS485, TTL) is disconnected due to an unspecified error.
    Communication is defined as all the Instruction Packet in the Dynamixel Protocol.
    Values
    Description
    Unit
    20[ms]
    Range
    0
    Deactivate Bus Watchdog Function, Clear Bus Watchdog Erro
    1 ~ 127
    Activate Bus Watchdog
    -1
    Bus Watchdog Error Status

    The Bus Watchdog function monitors the communication interval (time) between the controller and Dynamixel when Torque Enable (64) is '1'.
    If the measured communication interval (time) is larger than Bus Watchdog (98), the Dynamixel will be stopped. Bus Watchdog (98) will be changed to '-1' (Bus Watchdog Error).
    If the Bus Watchdog Error screen appears, the Goal Value (Goal PWM(100), Goal Current(102), Goal Velocity(104), Goal Position(116)) will be changed to read-only property.
    Therefore, when a new value is written to the Goal Value, a Range Error will be returned via the Status packet.
    If the value of Bus Watchdog (98) is changed to '0', Bus Watchdog Error will be cleared.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 7
    Last Post: 01-10-2016, 03:14 AM
  2. Arduino Library for Dynamixel XL-320 (and Dynamixel PRO if modified).
    By LuisGIII in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 06-07-2015, 11:00 PM
  3. New Feature: Gallery Profile Integration!!
    By Alex in forum Off Topic
    Replies: 0
    Last Post: 05-07-2008, 09:45 AM
  4. Discussion New audio/video embedding feature added - I NEED YOUR OPINION!!
    By Alex in forum Robotics General Discussion
    Replies: 27
    Last Post: 05-05-2008, 02:18 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •