Results 1 to 1 of 1

Thread: Electrical/Electronic and Mechanical Engineer for hire.

  1. #1
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,291
    Images
    27
    Rep Power
    276

    Electrical/Electronic and Mechanical Engineer for hire.

    Many years experience with Robotis products, numerous types of imaging hardware and software, and all sorts of electromechanical systems.

    I've been debating myself for quite some time whether to bring it up here, but the desperation is becoming overwhelming again. Among the personal projects that have been getting extensive design work for the last few weeks trying to take my mind off my long-term unemployed and soon to be flat-broke status:


    • star-networked, 10-channel, ~56Vdc LED controller for replacing all the 40+ year old fluorescent light fixtures in the basement with independently dimmable 'bulbs' magnetically attached to existing suspended ceiling frame
      • 16 Samsung LM561C LEDs in series per 'bulb' at <=150mA for up to ~1200 lumens each
      • Intended to be powered by 56V supply using 16S LiFePO4 backup pack (48~56V)
      • One wire for both half-duplex comms and ~12V controller power (GND, 12V/COMM, 56V)
      • All electrical connections using push-in, through-board connectors for clean and easy wiring
      • ATSAMD21E to utilize existing Arduino cores



    • servomotor in NEMA14 footprint with coreless BLDC motor, in-line 144:1 compound epicyclic gearhead, and ATSAMD21G (Arduino Zero) controller
      • Independent power supplies for motor (<=60V) and controller (12V~15V)
      • Magnetic absolute position encoder of output horn (Infineon TLV493D)
      • Low-side current sensing on all three phases (Allegro ACS711)
      • 34mm square by ~52mm long
        • four M3 mounting holes on a 26mm square on 34x34mm face to match NEMA14
        • multiple self-tapping M2x4mm mounting holes distributed along sides

      • Up to four SERCOM interfaces exposed
        • Current revision includes 3-pin TTL DXL, 4-pin RS-485 DXL, and two more UARTs with CAN transceiver ICs

      • Recently started working on alternative ATSAMD51G/E51J (Cortex-M4F at 120MHz) controller boards to ensure I can use a decent FOC algorithm to control the BLDC motor



    • small quad mech (fits within a 210x210x160mm box when stowed) based on 'Jameson' from GITS:SAC using NEMA14 servos fixed in the body and driving capstans to remotely control each DOF via dyneema tendons


    Also willing to part with Ripley - my slightly customized HROS-1 that I can rebuild into a stock HROS-1 with all electronics - as I have never made anywhere near as much progress on my gait engine as I had hoped.
    Last edited by tician; 04-10-2018 at 08:37 PM. Reason: indent/list formatting is not working correctly
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Standard servo electronic
    By fma in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 10-28-2015, 06:31 AM
  2. Core electrical engineering classes
    By Resilient in forum Off Topic
    Replies: 1
    Last Post: 04-24-2012, 12:45 PM
  3. Question(s) Electronic Brick to axon!
    By 123laurens in forum Robot Computers
    Replies: 4
    Last Post: 07-21-2010, 04:03 PM
  4. Electrical basics--need HELP!
    By mannyr7 in forum Mech Warfare
    Replies: 4
    Last Post: 05-31-2009, 12:26 PM
  5. Mechanical Engineer
    By valleycycles in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 01-13-2009, 07:45 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •