Page 1 of 3 123 LastLast
Results 1 to 10 of 23

Thread: Custom joystick to control robot arm

  1. Custom joystick to control robot arm

    Hello,

    I just wanted to share my latest project with the forum. I have created a custom input device to control movements on a robotic arm. I believe this kind of system is most commonly called a telemetry suit but in my case I don't think it could be called a suit.

    The input arm shows up as a standard windows joystick so it could be used for games or other applications as well however the input arm was designed to match the size and movements of the arm exactly. Some tweaking of the scales are needed especially for the base but it gives you an idea of what I was going for.

    Video:

    [ame="http://www.youtube.com/watch?v=zZwnyZPkylk"]YouTube - Controlling a robot arm naturally[/ame]


    I have created a video showing how easy the robot arm is to control when using this type of input device. A tutorial on how I did this exactly and what parts I used will come soon.

    Thanks for looking!
    Last edited by Alex; 08-22-2008 at 10:43 AM. Reason: attempt to fix the YouTube video

  2. #2
    Join Date
    May 2008
    Location
    WNC
    Posts
    413
    Images
    68
    Rep Power
    57

    Re: Custom joystick to control robot arm

    HakBot, welcome to the forum.
    Very cool stuff! That makes me want to drop all my current projects and build a telemetry suit!

  3. #3
    Join Date
    Jun 2008
    Location
    Crabfu's Garage.. <_<
    Posts
    302
    Images
    12
    Rep Power
    46

    Re: Custom joystick to control robot arm

    Very very cool! That is an amazing looking controller! +1 rep for sure!
    This ain't nothing but a summer jam
    Brown skin and cinnamon tans, whoa!
    This ain't nothing but a summer jam
    We're gonna party as much as we can
    Hey-yeah, ooh, hey-yeah
    Summer jam alright
    Hey-yeah, ooh, hey-yeah

  4. #4
    Join Date
    Apr 2008
    Location
    Nelson, New Zealand
    Posts
    1,356
    Images
    58
    Rep Power
    74

    Re: Custom joystick to control robot arm

    Ah, This is what I need for my Robotic arm prize, Look forward to your tutorial Hakbot.
    People yearn after this robotic dream, but you can't strip your life of all meaning, emotion and feeling and expect to function.


  5. #5
    Join Date
    Sep 2006
    Location
    Chicago Illinois
    Posts
    682
    Images
    174
    Rep Power
    85

    Re: Custom joystick to control robot arm

    Nicely done. I like the mini rover on your site too! Feel free to also post your tutorials in our tutorials section and linkback to your site as PR. (as long as the actual tutorial is here in full) You are doing some cool stuff.

  6. Re: Custom joystick to control robot arm

    Thanks for the kind words everyone. I will definitely be posting more in this forum!

  7. #7
    Join Date
    Apr 2008
    Location
    Sunnyvale, CA
    Posts
    378
    Images
    34
    Rep Power
    56

    Re: Custom joystick to control robot arm

    I love this! I always wanted one of those waldos from Andromeda Strain.

  8. #8

    Re: Custom joystick to control robot arm

    Love it... I hope to do something like that in the future.

  9. #9

    Re: Custom joystick to control robot arm

    Nice!!!! love that control, looks awesome!

    -Crabfu

  10. #10

    Re: Custom joystick to control robot arm

    Quote Originally Posted by HakBot View Post
    Hello,

    I just wanted to share my latest project with the forum. I have created a custom input device to control movements on a robotic arm. I believe this kind of system is most commonly called a telemetry suit but in my case I don't think it could be called a suit.
    Welcome to TRC! It's good to see you over here. You do very cool stuff! I watched the video, and it's amazing how this works. I did notice a little bit of the arm getting out of sync with the controller when you bring it back all the way. That could just be a calibration issue. With two of these on a robot with a camera, there would be some amazing possibilities..

    8-Dale
    I can handle complexity. It's the simple things that confound me.
    Do everything in moderation, ESPECIALLY, moderation..
    Sometimes the only way to win, is not to play.. -- Stephen Falken

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  2. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  3. Contest Entry Butler Robot
    By airman00 in forum Project Showcase
    Replies: 11
    Last Post: 07-31-2008, 09:28 PM
  4. How To Radio Control DC Motors Cheaply
    By Al1970 in forum Robotics General Discussion
    Replies: 1
    Last Post: 06-29-2008, 09:10 AM
  5. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •