Results 1 to 6 of 6

Thread: Pan and Tilt Kit Interface

  1. Pan and Tilt Kit Interface

    I am getting a pan and tilt kit from here, a problem is that, where can i download the library or the intrface to communicate from my c# code to the pan and tilt kit with servo motors?

  2. #2
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Pan and Tilt Kit Interface

    There are many P&T kits here, and without a link or PN, it's hard to guess for sure which one you are talking about..

    But, I'm assuming you're talking about this one:

    http://www.trossenrobotics.com/store...-Tilt-Kit.aspx

    The .NET library needed to interact with the PhidgetServo Controller can be downloaded directly from Phidgets':

    http://www.phidgets.com/downloads.php?os_id=1

    keep in mind though, this isn't software that's a direct interface with the P&T. It's simply a demo app used to demonstrate the features of the 4-motor PhidgetServo Controller.

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  3. Re: Pan and Tilt Kit Interface

    thanks for the reply,
    Yes, what i meant was the product you linked to.

    i checked it out, but could you please tell me which class should i look at, cause there are amny servo classes, and also motor classes in phidgets..


    thank you

  4. #4
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Pan and Tilt Kit Interface

    I think the doc sheet will help ya out a lot:

    http://www.phidgets.com/documentatio...uct_Manual.pdf

    Scroll down to page 8 and you'll see a C# app. The class that you want is Phidgets.Servo

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  5. #5
    Semicton Guest

    Re: Pan and Tilt Kit Interface

    Hey Sunjava,

    You can check out the upload section here and play around with this: http://forums.trossenrobotics.com/do...do=file&id=107 to help you get started. The demo only uses the first servo on the your board. It's using the Phidgets.Servo class.

  6. Re: Pan and Tilt Kit Interface

    just notice the price 105 US, thats no problem but the delivery charge doubled it up tp 194 US dollar..

    Still have to buy though

    thanks for the reply

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry Wall-E
    By 4mem8 in forum Project Showcase
    Replies: 218
    Last Post: 03-29-2009, 04:06 AM
  2. Project Pan and Tilt Shooting Gallery
    By Alex in forum Robotics General Discussion
    Replies: 1
    Last Post: 07-30-2008, 11:48 AM
  3. Making a Pan Tilt work with Joy stick
    By Daniel in forum Software and Programming
    Replies: 36
    Last Post: 06-14-2008, 10:14 AM
  4. Project Wii nunchuck + Arduino controlling a Pan and Tilt Camera
    By Alex in forum Robotics General Discussion
    Replies: 15
    Last Post: 04-29-2008, 10:06 AM
  5. Programing the Parallax Servo Controller (USB)
    By MinyFly92 in forum Software and Programming
    Replies: 7
    Last Post: 03-10-2008, 08:02 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •