Results 1 to 7 of 7

Thread: Poor quality of PhantomX Reactor slewing ring?

  1. Poor quality of PhantomX Reactor slewing ring?

    We've just built a PhantomX Reactor and the slewing ring appears to be really poor quality. It does not spin freely, has visible gaps in the visible ball race, the centre moves around horizontally relative to the outer ring and the motion even "sticks" at certain points. It seems a terribly poor quality part compared to the rest of the kit. Is this expected, or have we received something particularly substandard here? It's certainly not at all impressive.

  2. #2

    Re: Poor quality of PhantomX Reactor slewing ring?

    If it "doesn't work" then something's probably off.

    However, the Reactor is a low-cost AX-12 based arm. I wouldn't expect it to use the same $200+ slew bearings that you'd find in industrial automation equipment.

  3. Re: Poor quality of PhantomX Reactor slewing ring?

    What does "something's probably off" mean, really? I do have a bad bearing?

    Certainly I don't expect a $600 arm to have a $200 bearing - that would be ridiculous. But this bearing is so poor that I can't imagine it actually cost even $2 and as such a $600 robot is hobbled by this one very low quality part.

    What I'd like to know is how smooth-running are other people's slew rings on the PhantomX Reactor.

  4. #4

    Re: Poor quality of PhantomX Reactor slewing ring?

    Have you contacted Trossen, either by phone or email? Maybe there was a defective part...

  5. Re: Poor quality of PhantomX Reactor slewing ring?

    @kurteck - I haven't contacted Trossen about this particular issue yet (other issues with PhantomX reactor, I have, and no responses yet). I was hoping for a bit of feedback as to the general quality of the part here first. After some "running in" it's working to a "sticky" but workable level, but actually I'd like to have a "really good" quality bearing here instead of this crappy thing, even if not supplied through Trossen. Would anyone know of sources for suchlike?

  6. #6

    Re: Poor quality of PhantomX Reactor slewing ring?

    Sorry, I am not much help there. I have one of their Arms, that I received when they first were coming out. I have not done much with it in a long time. I sometimes use it to test out some software controller stuff, but that is about it. Hopefully someone else will have some ideas on different options

  7. #7

    Re: Poor quality of PhantomX Reactor slewing ring?

    I like vxb.com for bearings: http://www.vxb.com/SearchResults.asp...h=slew+bearing
    Another name for slew bearings is "slewing rings."
    You may be able to get away with a thrust bearing rather than a full slew ring, though, which would be cheaper: http://www.vxb.com/Thrust-Needle-Rol...p/kit12679.htm
    (I think a 7/8" ID bearing will fit pretty well around the horn of an AX-12 servo, but make sure to measure yourself for best results.)
    You may also be able to use a conical / tapered roller bearing, typically used for drive axles, if you can fit it appropriately.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX Reactor, ROS, MoveIt
    By Adam Glass in forum Interbotix Robotic Arms
    Replies: 7
    Last Post: 08-21-2017, 11:57 AM
  2. ROS Port of Commander.ino for PhantomX Reactor Arm
    By ramabrahma in forum ROS - Robot Operating System
    Replies: 1
    Last Post: 07-04-2013, 07:24 PM
  3. Playing with the PhantomX Reactor
    By Xevel in forum Interbotix Robotic Arms
    Replies: 6
    Last Post: 03-16-2013, 06:24 PM
  4. 3D Model of the PhantomX Reactor Arm
    By nckswt in forum Interbotix Robotic Arms
    Replies: 5
    Last Post: 12-31-2012, 04:49 PM
  5. Kurt's PhantomX Reactor Robot Arm
    By KurtEck in forum Interbotix Robotic Arms
    Replies: 11
    Last Post: 12-10-2012, 05:11 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •