Results 1 to 3 of 3

Thread: Arbotix-M control with a RC radio

  1. Arbotix-M control with a RC radio

    Hi,

    I'm pretty new to building robotics, and am building the WidowX arm right now. I want to control the arm with a radio controller I already own, from other hobbies. It has a lot of switches that I would like to bind to certain arm movements.

    The plan is to connect the Arbotix-M controller with analog inputs to the radio's receiver - and have preprogrammed movements that the arm performs. I think that I need to use the Arm Link software to "train" the robot and to have it's movements stored on the board. Is this the right way to go about it? Any ideas or suggestions would be appreciated.

    Thanks,
    spacerobo

  2. #2

    Re: Arbotix-M control with a RC radio

    It depends on what you want the RC to do. If you want direct control of the arm position from joysticks, you probably just write a sketch that receives RC pulses (or ibus protocol if that's the kind of receiver you have) and translates them to desired servo positions, then sends those servo positions.
    If you want to have pre-canned positions/poses of the arm, and let different buttons on the remote control go to those positions, then "training" positions might make sense.

  3. Re: Arbotix-M control with a RC radio

    I was hoping to do canned poses, because I'll be using the control joysticks for the vehicle its mounted to. I think I'll use the armlink program to start learning how to train poses before coding them myself - but I can't for the life of me get it to work standalone... its missing some sort of file. Do you have any experience with that?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) How to control Arbotix-m through Labview?
    By asdkaresz in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 01-18-2018, 01:43 PM
  2. PID Control for Dynamixel servos using Arbotix-M
    By navidahmeduom in forum Arbotix, Microcontrollers, Arduino
    Replies: 6
    Last Post: 05-20-2015, 11:15 AM
  3. Replies: 1
    Last Post: 03-22-2013, 11:44 PM
  4. How To Radio Control DC Motors Cheaply
    By Al1970 in forum Robotics General Discussion
    Replies: 1
    Last Post: 06-29-2008, 10:10 AM
  5. Kondo Radio Control Question
    By evaderdjo in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 06-07-2008, 01:43 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •