Results 1 to 5 of 5

Thread: Walker with built-in Segway?

  1. #1

    Walker with built-in Segway?

    I want to build a new robot!

    https://www.youtube.com/watch?v=-7xvqQeoA8c

    But it doesn't actually count as walker for 'mech warfare...

  2. #2

    Re: Walker with built-in Segway?

    Where can I get those kinds of wheels, btw (perhaps smaller) with a fixed hub, not an axle?
    All the kid bike / trike wheels have axles, and I'd want to mount on a motor shaft.

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,253
    Images
    27
    Rep Power
    273

    Re: Walker with built-in Segway?

    I would not be surprised if they milled their own rims and cast the tread onto the rim. Very easy to do and not super expensive. Can even go with 3D printed hubs and molds like on several 250lbs class robots.

    If you must go 'off the shelf', usually have to buy a rim designed for mounting external sprocket or disc brake that rides on a solid axle via bearings and just connect the motor through a belt/chain. Otherwise go with a solid (molded plastic or cast metal) hub/rim and bearings, then press out the bearings and replace them with a spline/shaft adapter. Surplus Center sometimes has small-ish diameter wheels with solid molded rims ready to mate to a splined shaft.

    'Hoverboard' rims/wheels might be an option.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  4. #4

    Re: Walker with built-in Segway?

    Oh, hoverboards!
    I can get motor and wheel all-in-one. Just hook up a three-phase controller and I'm ready to go!
    https://amzn.to/2M93Yni

    Maybe these wheels would be good for a higher-speed Money Pit, too?

  5. #5

    Re: Walker with built-in Segway?

    Although the specs are hilarious:

    Code:
    Voltage: 36V
    Load current: 0.6-0.9A
    Power: 350W



Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. R-team panels available built?
    By jwatte in forum Mech Warfare
    Replies: 5
    Last Post: 03-27-2017, 01:21 PM
  2. Camer is built but were to plug it in.
    By LloydF in forum HR-OS1 Development and Discussion
    Replies: 34
    Last Post: 06-07-2015, 04:44 PM
  3. Built my quadruped. Not really sure where to go next
    By 2zon in forum Humanoids, Walkers & Crawlers
    Replies: 17
    Last Post: 10-10-2013, 10:19 AM
  4. Scratch built hex
    By MaconSwift in forum Robotics General Discussion
    Replies: 3
    Last Post: 01-20-2010, 01:49 PM
  5. Humanoid Segway
    By asbrandsson in forum Project Showcase
    Replies: 0
    Last Post: 03-12-2009, 07:04 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •