Page 2 of 2 FirstFirst 12
Results 11 to 12 of 12

Thread: avrdude: verification error, first mismatch

  1. Re: avrdude: verification error, first mismatch

    Quote Originally Posted by jwatte View Post
    When you use an ISP programmer, you do NOT typically use a serial port, and you do NOT typically use serial communication.
    Instead, use the "upload using programmer" option.
    (There are some programmers that are serial, but most use a USB protocol, such as USBTiny, or USBAsp, or somesuch.)
    Thank you for responding, but if you look at the image number 6, you can see how I used the option to load using programmer.

  2. Re: avrdude: verification error, first mismatch

    Quote Originally Posted by KurtEck View Post
    I could not tell from your pictures if this is the same ISP Programmer that Trossen sells? If it is than the AVRSPI mkII (serial)
    Is the correct Programmer to choose and you do need to select the appropriate COM port for it.

    I should again try to digg up my setup... Not sure where it is sitting right now as I am not doing anything these days with the Arbotix boards.
    Yes, it is the same ISP Programmer.

    I tried the two COM ports that came out...

Thread Information

Users Browsing this Thread

There are currently 4 users browsing this thread. (1 members and 3 guests)

  1. jt16

Similar Threads

  1. Question(s) Avrdude error - Artibotix - board not working
    By vali in forum Arbotix, Microcontrollers, Arduino
    Replies: 8
    Last Post: 03-26-2018, 11:34 AM
  2. Question(s) ArbotiX avrdude error
    By arbotix in forum Software and Programming
    Replies: 4
    Last Post: 08-19-2017, 02:49 AM
  3. avrdude.exe stk500_getsync() not in sync error
    By mycroft in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 09-28-2016, 01:47 PM
  4. avrdude : verification error
    By amir204 in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 09-29-2015, 04:09 AM
  5. Issues with Arbotix Programming- avrdude: stk500_getsync() error
    By Nitro in forum Software and Programming
    Replies: 4
    Last Post: 12-11-2012, 01:41 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •