Page 2 of 2 FirstFirst 12
Results 11 to 16 of 16

Thread: avrdude: verification error, first mismatch

  1. Re: avrdude: verification error, first mismatch

    Quote Originally Posted by jwatte View Post
    When you use an ISP programmer, you do NOT typically use a serial port, and you do NOT typically use serial communication.
    Instead, use the "upload using programmer" option.
    (There are some programmers that are serial, but most use a USB protocol, such as USBTiny, or USBAsp, or somesuch.)
    Thank you for responding, but if you look at the image number 6, you can see how I used the option to load using programmer.

  2. Re: avrdude: verification error, first mismatch

    Quote Originally Posted by KurtEck View Post
    I could not tell from your pictures if this is the same ISP Programmer that Trossen sells? If it is than the AVRSPI mkII (serial)
    Is the correct Programmer to choose and you do need to select the appropriate COM port for it.

    I should again try to digg up my setup... Not sure where it is sitting right now as I am not doing anything these days with the Arbotix boards.
    Yes, it is the same ISP Programmer.

    I tried the two COM ports that came out...

  3. #13

    Re: avrdude: verification error, first mismatch

    Again not sure what to tell you. It looks like your setup is correct.

    I could not tell what version of Arduino you are using. Probably should not mater.

    I did drag out my setup, which is using the same programmer (Pololu) it created COM8 and COM9 and on my machine Com8 is the right one.

    I was able to burn bootloader and I was able to upload blink (changing pin to 0) using upload using programmer and that worked.

    So the only thing now would be to contact Trossen Support. See if they will send you a new board?

    Again these days I would not recommend buying these boards for many reasons, but would probably stir you to some better supported boards like openCM9.04... As if you look up at Trossen's website you will see their new Arms are now shipping with these!

  4. Re: avrdude: verification error, first mismatch

    Thank you very much, you have been helpful.


    I bought another Arbotix, because in one month I have to present my project, and I have everything done for Arbotix and I do not have time to change.


    For the next project, I will use openCM9.04.

    Best Regards!!

  5. Re: avrdude: verification error, first mismatch

    Good afternoon again.


    I have already bought my new Arbotix, but I want to try one last thing to try to fix the one that is broken.


    I want to reinstall the firmware. Can someone tell me where I can download it? Is there any guidance I can follow? Could you advise me how to do it?


    I have already installed the Atmel Studio 7.0


    Thank you very much.
    Last edited by jt16; 08-16-2018 at 11:03 AM.

  6. #16

    Re: avrdude: verification error, first mismatch

    The only firmware for this is the Bootloader. Which is what Arduino command is trying to do.

    And on my machine the Arduino install that I am using (My own for 1.8.5), the files are installed at:
    C:\Users\kurte\Documents\Arduino\hardware\arbotix\ avr\bootloaders\atmega644p

    Which are up in my Fork/Branch of the Arbotix project:
    https://github.com/KurtE/arbotix/tre...ers/atmega644p

    Probably same binaries exist in all of the branches/forks...

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Avrdude error - Artibotix - board not working
    By vali in forum Arbotix, Microcontrollers, Arduino
    Replies: 8
    Last Post: 03-26-2018, 11:34 AM
  2. Question(s) ArbotiX avrdude error
    By arbotix in forum Software and Programming
    Replies: 4
    Last Post: 08-19-2017, 02:49 AM
  3. avrdude.exe stk500_getsync() not in sync error
    By mycroft in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 09-28-2016, 01:47 PM
  4. avrdude : verification error
    By amir204 in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 09-29-2015, 04:09 AM
  5. Issues with Arbotix Programming- avrdude: stk500_getsync() error
    By Nitro in forum Software and Programming
    Replies: 4
    Last Post: 12-11-2012, 01:41 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •