Page 2 of 4 FirstFirst 1234 LastLast
Results 11 to 20 of 40

Thread: The task (lawn mower topic)

  1. #11

    Re: The task (lawn mower topic)

    seems like a motor brush problem(spring broken).
    That's unfortunate!
    I am more and more becoming a fan of brushless motors ....
    They're as robust as steppers, but faster and higher power!

  2. Re: The task (lawn mower topic)

    While waiting on parts to repair my motor, got to thinking about plan B.

    Click image for larger version. 

Name:	Cap2.jpg 
Views:	17 
Size:	44.2 KB 
ID:	7275
    some of these type devices have a 500m range.
    found one on ebay with 250m outdoors range for $60.00
    almost seems like it should be a plan A, but because of costs, it's
    still a plan B.


    Tommy

  3. Re: The task (lawn mower topic)

    got the brushes, but wrong size.
    because the springs failed on the brushes from the motor
    I has able to remove springs from new brushes and put
    them on my old brushes, and get the motor to run.

    I was able to test the record/playback software. while it did
    function as planed, it could not repeat angles to required tolerance.

    the platform has about 6deg of lost motion in the drive train(gears,sprockets,chains)
    so some type of angle feedback is needed.

    Tommy

  4. #14

    Re: The task (lawn mower topic)

    6 degrees is a fair amount! I imagine you already tightened up everything you can?
    If you wiggle it, can you see what the limiting factor is?

  5. Re: The task (lawn mower topic)

    can you see what the limiting factor is?
    Click image for larger version. 

Name:	cap3.PNG 
Views:	10 
Size:	401.5 KB 
ID:	7278

    the motor gearbox has 2deg of lost motion in them.
    a few years ago I opened one of these type gearboxes
    and pinned it's internal gears to their shafts and was
    able to reduce it to .5degs, but because chains stritch
    and motor brackets can move with heavy loads I gave
    up on that approach.

    that's when I came up with the below idea.

    Click image for larger version. 

Name:	pic3b.jpg 
Views:	19 
Size:	122.9 KB 
ID:	7277

    This device gives me .008deg resolution of the angle
    the device is moving(Q axis). it also lets the platform
    make sweet crop circles.

    this device has limitations. (losing contact with the ground, and the math is convoluted)


    Tommy
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	pic3.jpg 
Views:	6 
Size:	136.0 KB 
ID:	7276  
    Last edited by Tommy_T; 08-11-2018 at 06:53 AM.

  6. Re: The task (lawn mower topic)

    While waiting on cash flow(payday), I had a very strong LED light sitting around
    so I tested using it as a target, see if my cheap webcam could pick it up from
    1000ft.

    My cellphone camera could pick it up.
    Click image for larger version. 

Name:	IMG_4729.jpg 
Views:	15 
Size:	136.9 KB 
ID:	7279Click image for larger version. 

Name:	IMG_4730.jpg 
Views:	15 
Size:	92.2 KB 
ID:	7280Click image for larger version. 

Name:	IMG_4734.jpg 
Views:	14 
Size:	242.4 KB 
ID:	7281

    But, not my webcam.

    Click image for larger version. 

Name:	IMG_4736.jpg 
Views:	17 
Size:	89.8 KB 
ID:	7282

    Tommy

  7. #17

    Re: The task (lawn mower topic)

    Oh, that's nice!

    If losing contact is a problem, I bet a Raspberry Pi + camera pointed down can, in a pinch, be turned into a picture-based visual odometer. I've wanted to try that, but never gotten around to it. (I believe that downwards-facing cameras for slow speeds can be more accurate than the general-purpose cars-on-streets visual odometers that have significant drift.)

  8. Re: The task (lawn mower topic)

    I bet a Raspberry Pi + camera pointed down can, in a pinch, be turned into a picture-based visual odometer.
    Jwatte, monocular visual odometry off loaded on a Pi seems like a fun test, but I'm still looking at mechanical methods
    of getting reliable odometry information.

    I'm currently testing a 6" #40 chain sprocket.

    Click image for larger version. 

Name:	pic4.jpg 
Views:	13 
Size:	107.8 KB 
ID:	7283

    I get .015" resolution with current setup.

    Tommy

  9. Re: The task (lawn mower topic)

    The next test is finding the maximum distance my webcam can
    reliable pick up an LED TARGET. The corps(corn this year) make
    a sweet target, but they are not always there.



    Tommy

  10. #20

    Re: The task (lawn mower topic)

    Having the LED be the "brightest thing" seems hard. Can you recognize some blinking pattern instead? Of course there will be latency for that, but that might not be so bad.

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. Lawn Mower [?] Project
    By Nikhil Thiruvengadam in forum Software and Programming
    Replies: 6
    Last Post: 05-07-2010, 08:47 PM
  2. Way off topic. Any Musicians here?
    By Quantum in forum Off Topic
    Replies: 5
    Last Post: 03-17-2010, 09:29 PM
  3. Replies: 6
    Last Post: 02-02-2010, 05:52 AM
  4. New Mower Project
    By a1programmer in forum Robotics General Discussion
    Replies: 4
    Last Post: 09-30-2009, 09:25 AM
  5. "ALMower" [was: Robotic Lawn Mower]
    By revoltage in forum Robotics General Discussion
    Replies: 363
    Last Post: 07-19-2009, 08:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •