Page 5 of 7 FirstFirst 1234567 LastLast
Results 41 to 50 of 66

Thread: The task (lawn mower topic)

  1. #41

    Re: The task (lawn mower topic)

    this season's build is a little different.

    while driving around chicago I noticed people using stand up lawn mowers,
    to find out why, what's the benefit I could have stopped and asked, but that's
    not the way I fly, this season the gravely mowing deck is going stand up.

    but because I wanted one handed operations I'll go with a steering wheel setup
    for on-board control.

    the colored buttons are for speed control.

    Click image for larger version. 

Name:	IMG_5547.jpg 
Views:	54 
Size:	108.0 KB 
ID:	7510
    Click image for larger version. 

Name:	IMG_5548.jpg 
Views:	55 
Size:	111.3 KB 
ID:	7511
    Click image for larger version. 

Name:	IMG_5550.jpg 
Views:	54 
Size:	141.4 KB 
ID:	7512
    Click image for larger version. 

Name:	IMG_5553.jpg 
Views:	52 
Size:	103.8 KB 
ID:	7513
    Click image for larger version. 

Name:	IMG_5554.jpg 
Views:	53 
Size:	128.5 KB 
ID:	7514
    Click image for larger version. 

Name:	IMG_5559.jpg 
Views:	53 
Size:	116.4 KB 
ID:	7515
    Click image for larger version. 

Name:	IMG_5560.jpg 
Views:	55 
Size:	90.5 KB 
ID:	7516
    Click image for larger version. 

Name:	IMG_5565.jpg 
Views:	59 
Size:	112.5 KB 
ID:	7517

  2. #42

    Re: The task (lawn mower topic)

    Neat!

    Those round colored push buttons from E-switch are favorites of mine, btw :-)

  3. #43

    Re: The task (lawn mower topic)

    Jwatte , I do hope they work better then the two position switches I got from Amazon also,
    which failed (sometimes worked, sometimes not)
    hard to complain when you buy 5 for 12.00 and free shipping

    I ordered some more but picked the 2 for 12.00 option

    I'm using them on the ignition system of the gas engine, sucks when the engine randomly quits

    plan C is to get them from McMastercarr , they always seemed to work fine, but cost about $30.
    Last edited by Tommy_T; 05-08-2019 at 07:09 AM.

  4. #44

    Re: The task (lawn mower topic)

    with the alternator installed and charging the batteries, this task is almost
    complete(just need to clean up wiring and make covers for the batteries) .

    Click image for larger version. 

Name:	IMG_5633.jpg 
Views:	43 
Size:	87.3 KB 
ID:	7555

    Click image for larger version. 

Name:	IMG_5637.jpg 
Views:	45 
Size:	86.1 KB 
ID:	7556

    Click image for larger version. 

Name:	IMG_5721.jpg 
Views:	44 
Size:	157.3 KB 
ID:	7557

    Click image for larger version. 

Name:	IMG_5738.jpg 
Views:	46 
Size:	94.3 KB 
ID:	7558

    Click image for larger version. 

Name:	IMG_5743.jpg 
Views:	161 
Size:	120.2 KB 
ID:	7559

    Click image for larger version. 

Name:	IMG_5640.jpg 
Views:	47 
Size:	105.7 KB 
ID:	7560

    Click image for larger version. 

Name:	IMG_5612.jpg 
Views:	150 
Size:	131.3 KB 
ID:	7561

  5. #45

    Re: The task (lawn mower topic)

    I have read and re-read all the posts from the beginning of this thread and the "Mule" thread.
    I am truly impressed with your projects and your accomplishments. Congrats!
    Big bots are the best bots!
    I am hoping you will be sharing updates soon since it is the heart of mowing season now.
    On the edge of my seat awaiting your next update.
    I reject your reality and inject my own.

  6. #46

    Re: The task (lawn mower topic)

    I am hoping you will be sharing updates
    EdZachery, you are correct about it being heart of the mowing season, but now
    I'm dealing with the heat of the mowing season, as it turns out alternators get
    damn hot. I installed a temperature probe on it and after mowing an acre of
    grass on hilly areas the alternator can get to 250degF (120c) which is hot
    enough to melt cheap wire insulation.

    my current plan is to try to cool the alternators with air.
    a 270cfm 12vdc fan should be here tomorrow

    all-in-all I'm sold on using alternators for extending the run time of these bigger
    projects, the Mule is also getting one.

  7. #47

    Re: The task (lawn mower topic)

    Yikes, that is hot. The fan should definitely help. It looks like you have plenty of room for some "IHS" (Improvised Heat Shield) as well.
    Thank you for the update! I will be looking forward to more.
    I reject your reality and inject my own.

  8. #48

    Re: The task (lawn mower topic)

    while I picked this task because I was thinking it would go fast(faster then most tasks I pick)(some last years).
    so I'd have time to finish the four wheel drive system on the mule before winter
    gets here. but, I found a new ELO 7" touchscreen on ebay for $80, and I have
    some ultrasonic sensors that I want to test for keeping the mowing deck from
    hitting walls and fences(the mower deck is 1/4" steel, anything it hits breaks)
    and I spend a lot of time mowing along buildings and fences.

  9. #49

    Re: The task (lawn mower topic)

    I should now be able to test to see if moving 270cfm of air across the alternator
    can control the temperature it operates at.

    Click image for larger version. 

Name:	IMG_5796.jpg 
Views:	36 
Size:	111.1 KB 
ID:	7565

    Click image for larger version. 

Name:	IMG_5798.jpg 
Views:	35 
Size:	113.3 KB 
ID:	7566

    Click image for larger version. 

Name:	IMG_5800.jpg 
Views:	39 
Size:	115.0 KB 
ID:	7567

  10. #50

    Re: The task (lawn mower topic)

    That's a fair bit of air :-D
    At that point, the limiting factor may be the surface area of the alternator casing.
    Which leads you to consider water channels, ....

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Lawn Mower [?] Project
    By Nikhil Thiruvengadam in forum Software and Programming
    Replies: 6
    Last Post: 05-07-2010, 08:47 PM
  2. Way off topic. Any Musicians here?
    By Quantum in forum Off Topic
    Replies: 5
    Last Post: 03-17-2010, 09:29 PM
  3. Replies: 6
    Last Post: 02-02-2010, 05:52 AM
  4. New Mower Project
    By a1programmer in forum Robotics General Discussion
    Replies: 4
    Last Post: 09-30-2009, 09:25 AM
  5. "ALMower" [was: Robotic Lawn Mower]
    By revoltage in forum Robotics General Discussion
    Replies: 363
    Last Post: 07-19-2009, 08:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •