Page 6 of 6 FirstFirst ... 23456
Results 51 to 58 of 58

Thread: The task (lawn mower topic)

  1. #51

    Re: The task (lawn mower topic)

    Jwatte, I have room to mount a second blower on the other side, that would
    give me 540cfm of air on the alternator and woulds only cost 6amps of power at 24vdc.

    I don't know if the high heat is caused by an undersized alternator(50amp) or the
    high load placed on it (the motors are drawing 100amps from the batteries at times),
    or that it's just a cheap alternators($120.00).

    I know it's not the bearings, because it runs at 20 deg f over ambient with no load(not excited).

    I found a 24v 100amp alternator on ebay that I could give a try.

    because the blower(s) only need to operate when the engine is running the
    noise they make shouldn't cause me an issue(mower sounds like a vacuum cleaner when blower is on)
    Last edited by Tommy_T; 1 Week Ago at 08:18 PM.

  2. #52

    Re: The task (lawn mower topic)

    Many alternators have a regulator built in, and that regulator is, as far as I can tell, a linear regulator, meaning they sink a bunch of heat to the case when they would generate more voltage than the application draws.
    I wouldn't be surprised at all if the alternator heat came from the regulator, and not from anything mechanical!
    If that were the case, then using an unregulated alternator, and using a DC DC converter built to regulate battery charge from a varying input (high input voltage noise rejection) might help significantly.
    I guess one way of figuring out whether this is the case is to disconnect the alternator output (so it free runs) and see if it still gets hot when you run on batteries only?

  3. #53

    Re: The task (lawn mower topic)

    I may have found the issue with the alternator, it seems these are single wire devices,
    that self excite, but I wired the excite input to 24vdc when the engine is running.

    that could over ride the alternator's voltage regulator(maybe).

    while air movement may not be the fix for the alternator issue spending a little time on
    it could help me down the road.

    Click image for larger version. 

Name:	IMG_5803.jpg 
Views:	6 
Size:	75.5 KB 
ID:	7568

    Click image for larger version. 

Name:	IMG_5810.jpg 
Views:	8 
Size:	126.8 KB 
ID:	7569

  4. #54

    Re: The task (lawn mower topic)

    with the blower running the servo motors are operating about 30degf cooler.

  5. #55

    Re: The task (lawn mower topic)

    That sounds pretty good!

  6. #56

    Re: The task (lawn mower topic)

    Crap, the alternator is at 85degf while mower is running, and batteries lasted 30min. ,
    that means alternator is cooked.

  7. #57

    Re: The task (lawn mower topic)

    Thinking the alternator in the image below with it's fan internal may keep
    cooler with 500+ cfm of air movement then the enclosed type I tried first.

    maybe.

    today the outside temps reached 90degf. after 30min of mowing with both blowers
    running the servo motors read 117degf on right motor 122degf on the left servo motor.

    before the blowers at 75degf outside temp. I'd see 150degf on the left and 170degf on the right.


    Click image for larger version. 

Name:	IMG_5815.jpg 
Views:	5 
Size:	112.7 KB 
ID:	7573

    Click image for larger version. 

Name:	IMG_5817.jpg 
Views:	6 
Size:	128.6 KB 
ID:	7574

    Click image for larger version. 

Name:	IMG_5818.jpg 
Views:	5 
Size:	115.0 KB 
ID:	7575
    Last edited by Tommy_T; 1 Day Ago at 02:40 PM.

  8. #58

    Re: The task (lawn mower topic)

    seems like a motor brush problem(spring broken).
    I know the feeling!

    WHY ... CAN'T ... THINGS ... STAY ... WORKING !?!?!?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Lawn Mower [?] Project
    By Nikhil Thiruvengadam in forum Software and Programming
    Replies: 6
    Last Post: 05-07-2010, 08:47 PM
  2. Way off topic. Any Musicians here?
    By Quantum in forum Off Topic
    Replies: 5
    Last Post: 03-17-2010, 09:29 PM
  3. Replies: 6
    Last Post: 02-02-2010, 05:52 AM
  4. New Mower Project
    By a1programmer in forum Robotics General Discussion
    Replies: 4
    Last Post: 09-30-2009, 09:25 AM
  5. "ALMower" [was: Robotic Lawn Mower]
    By revoltage in forum Robotics General Discussion
    Replies: 363
    Last Post: 07-19-2009, 08:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •