Page 1 of 8 12345 ... LastLast
Results 1 to 10 of 71

Thread: The task (lawn mower topic)

  1. #1

    The task (lawn mower topic)

    The task

    Automatically mow a field 100ft x 1000ft.

    Task started: 4/2018
    Task Completed:
    Click image for larger version. 

Name:	IMG_4693.jpg 
Views:	334 
Size:	132.8 KB 
ID:	7258

    The tool.
    Click image for larger version. 

Name:	IMG_4696.jpg 
Views:	569 
Size:	153.2 KB 
ID:	7259

    I found the mowing deck on Craig's list 3 months ago,
    the engine was blown so the mower deck only cost me
    $300, then I found an 14.5hp Briggs engine on Craig's
    list for $120 and with a little searching I also found an
    electric PTO clutch that fit the engine for $60.
    Click image for larger version. 

Name:	mower1.PNG 
Views:	330 
Size:	392.0 KB 
ID:	7255 Click image for larger version. 

Name:	mower2.PNG 
Views:	321 
Size:	523.2 KB 
ID:	7256 Click image for larger version. 

Name:	mower3.PNG 
Views:	309 
Size:	226.5 KB 
ID:	7257

    the next thing I need to find is a 24Vdc alternator. the briggs engine has
    a 9 Amp 12vdc alternator to charge the battery for the 12vdc system(PTO clutch, Arduino(2), Lights, PC and starting engine).
    The Electric drive system is 24vdc.

    Electric Drive System:
    (1) Sabertooth 2x60 with the V2(kangaroo) motion control board.(Serial interface)
    (2) 1000 watt electric wheelchair motors with encoders.($150 from Ebay, sweet!)

    Control System( Manual Mode ):
    (1) Arduino Mega
    (1) Arduino Nano (Safety System)
    (2) XBee-PRO 900HP

    Control System ( Automatic ):
    (1) Lanovo S10 laptop PC (Windows XP)
    (1) US Digital USB4 device(I/Os, encoder cards, analogs)

    Current Senors:
    (1) Yocto-GPS
    (1) Yocto-D3
    (2) Encoders (odometer, Direction)



    Tommy
    Last edited by Tommy_T; 07-31-2018 at 08:50 AM.

  2. #2

    Re: The task (lawn mower topic)

    Looks like a fun, real-world system!
    How much fabrication experience do you have? Do you have machining tools?
    I'd love to see more about how this project goes!

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,316
    Images
    27
    Rep Power
    280

    Re: The task (lawn mower topic)

    Quote Originally Posted by jwatte View Post
    Looks like a fun, real-world system!
    How much fabrication experience do you have? Do you have machining tools?
    I'd love to see more about how this project goes!
    This is Tommy_T we're talking about, jwatte. It's another developmental stage of the Magnificent Mule; autonomous instead of human control through FPV or direct viewing from the porch.


    Not sure I would trust any of my code to safely on a platform equipped with a proper gas-powered mower deck. I would definitely have to build a collision sensor system around the bot's perimeter to ensure nothing ever gets near the blades.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  4. #4

    Re: The task (lawn mower topic)

    It's another developmental stage of the Magnificent Mule
    tician, I see it as too big a task for the mule. the mule is just not fast enough.

    this platform is designed for mowing speeds needed to do 3 acres in 6 hours.
    and with the gas engine also strong enough to charge the battery packs they can
    be greatly reduced in size and weight.

    this platform is also using servo motors for it's drive system.

    the Mule System is waiting for snow.
    Click image for larger version. 

Name:	DSC07343.JPG 
Views:	315 
Size:	127.3 KB 
ID:	7261


    Tommy

  5. #5

    Re: The task (lawn mower topic)

    It can't be said I didn't give an electric mowing deck a try.
    Click image for larger version. 

Name:	DSC06451.JPG 
Views:	319 
Size:	111.0 KB 
ID:	7262Click image for larger version. 

Name:	DSC07552.JPG 
Views:	325 
Size:	153.5 KB 
ID:	7263Click image for larger version. 

Name:	DSC08359.JPG 
Views:	327 
Size:	170.6 KB 
ID:	7264Click image for larger version. 

Name:	DSC08401.JPG 
Views:	325 
Size:	166.1 KB 
ID:	7265
    Click image for larger version. 

Name:	george87.jpg 
Views:	329 
Size:	131.1 KB 
ID:	7266Click image for larger version. 

Name:	george201.jpg 
Views:	370 
Size:	200.4 KB 
ID:	7267

    but, after seeing what a 14hp gas engine can do with even very overgrown
    grass like the below image, I'm sold.
    Click image for larger version. 

Name:	IMG_4686.jpg 
Views:	327 
Size:	384.6 KB 
ID:	7268


    Tommy

  6. #6

    Re: The task (lawn mower topic)

    Not sure I would trust any of my code to safely on a platform equipped with a proper gas-powered mower deck.
    tician, this platform while using a different control protocol(serial), does use the same safety logic
    as the mule, which has demonstrated its worth countless times.

    It turns out these gas engines have a terminal on the coil of the ignition system that when ground is
    applied it stops the engine, so interfacing the engine kill to the control circuits is very straight forwards.
    also, the mower blades are controlled by an electric clutch, which is also easy to connect to the safety system.

    the electric clutch draw 5amps at 12vdc.
    the gas engine has a 9amp built-in generator.


    Tommy
    Last edited by Tommy_T; 08-06-2018 at 08:27 AM.

  7. #7

    Re: The task (lawn mower topic)

    Plan A:

    Click image for larger version. 

Name:	pic1.jpg 
Views:	315 
Size:	4.0 KB 
ID:	7270

    record a perfect sequence of going 100ft then turning 180deg to the left with a .5 ft overlap of
    last cut path, then going back 100ft and turning 180deg right with the overlap, then stop.

    Click image for larger version. 

Name:	IMG_4699.jpg 
Views:	346 
Size:	108.5 KB 
ID:	7271

    take an image with a webcam of a target area. using that image I should be able to correct any
    alignment issues from last cut path, then just rerun the last recorded path.

    the high contrast between sky and tree tops should come in handy.

    repeat 154 times.

    the pauses should come in handy as a way to control drive motor temperatures.
    it does get very hot out in the sun.


    Tommy
    Last edited by Tommy_T; 08-06-2018 at 10:00 AM.

  8. #8

    Re: The task (lawn mower topic)

    Because it's a known, surveyable area, you totally should use RTK GPS. You can get centimeter precision using just that!
    Adding vision and other sensors would be candy on top.

    Also, 14.5 HP is just, what, 11 kW? How much safety do you REALLY need for that anyway? :-D :-D

    Using LiFePo4 batteries as stabilizers for the alternator seems like a great idea, as long as you can avoid overcharging, presumably by shunting in some big resistive load of some sort (or turn off the alternator.)

  9. #9

    Re: The task (lawn mower topic)

    Because it's a known, surveyable area, you totally should use RTK GPS. You can get centimeter precision using just that!
    jwatte, I'm sure it would help, but not sure how it would handle tree lines the block sections of the sky(lost satellites) errors.

    I'm looking into it, thanks.

    Tommy

  10. #10

    Re: The task (lawn mower topic)

    Click image for larger version. 

Name:	pic2.jpg 
Views:	318 
Size:	153.8 KB 
ID:	7273

    Just as I was about to test the record/playback software one of my motors failed,
    seems like a motor brush problem(spring broken).

    Click image for larger version. 

Name:	IMG_4708.jpg 
Views:	324 
Size:	101.4 KB 
ID:	7274

    Tommy

Thread Information

Users Browsing this Thread

There are currently 6 users browsing this thread. (0 members and 6 guests)

Similar Threads

  1. Lawn Mower [?] Project
    By Nikhil Thiruvengadam in forum Software and Programming
    Replies: 6
    Last Post: 05-07-2010, 09:47 PM
  2. Way off topic. Any Musicians here?
    By Quantum in forum Off Topic
    Replies: 5
    Last Post: 03-17-2010, 10:29 PM
  3. Replies: 6
    Last Post: 02-02-2010, 06:52 AM
  4. New Mower Project
    By a1programmer in forum Robotics General Discussion
    Replies: 4
    Last Post: 09-30-2009, 10:25 AM
  5. "ALMower" [was: Robotic Lawn Mower]
    By revoltage in forum Robotics General Discussion
    Replies: 363
    Last Post: 07-19-2009, 09:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •