Results 1 to 2 of 2

Thread: Problem with control of Dynamixel AX-12A by using MatLab

  1. #1
    adamlevine Guest

    Problem with control of Dynamixel AX-12A by using MatLab

    I plan to work with Dynamixel AX-12A, which is connected to computer (Win64) by USB2Dynamixel. I use information from Dynamixel SDK Manual (item 4.6) for adding libraries in MatLab R2014a (it's files for DynamixelSDK-3.4.1), but when I run file "read_write.m", I got error:
    Index exceeds matrix dimensions.
    Error in
    loadlibrary>getLoadlibraryCompilerConfiguration
    (line 497)
    compilerConfiguration=compilerConfiguration(1);
    %unix machines return c and cpp
    compilers here
    Error in loadlibrary (line 253)
    [thunk_build_fn,preprocess_command]=getLoadlibraryCompilerConfiguration(ccinclude,hea der,headername,compilerConfiguration);
    Error in read_write (line 60)
    [notfound, warnings] =
    loadlibrary(lib_name,
    'dynamixel_sdk.h', 'addheader',
    'port_handler.h', 'addheader',
    'packet_handler.h');
    Also I tried to add library as it's written in ROBOTIS e-Manual v1.24.00, but I have simular error.
    Could you help me, what should I do?
    Last edited by adamlevine; 08-03-2018 at 08:07 PM.

  2. #2

    Re: Problem with control of Dynamixel AX-12A by using MatLab

    Sorry, I am not a matlab user so I don't know, maybe someone else up here might...

    I would suggest that you post issues like this up on the Robotis Forum: http://en.robotis.com/service/forum.php

    Their main forum person tries to answer most questions and/or direct you to where to get help.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Dynamixel AX-12A serially connected to MATLAB
    By riccardovasapolli in forum Robotics General Discussion
    Replies: 1
    Last Post: 04-12-2018, 05:06 PM
  2. Question(s) Delete
    By JimiH in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 05-11-2016, 07:55 AM
  3. Question(s) Dynamixel with Matlab
    By jek in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 09-05-2015, 11:33 AM
  4. Question(s) How to Set the Torque limit for Dynamixel MX-28 using MATLAB?
    By ubs3 in forum Software and Programming
    Replies: 1
    Last Post: 03-06-2015, 08:41 PM
  5. Need matlab code for negative rotation of Dynamixel AX-12+
    By ngom52 in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 03-12-2010, 01:50 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •