Results 1 to 3 of 3

Thread: Vertical movement sensor

  1. Vertical movement sensor

    Hi,

    I am wondering if anyone knows a sensor that only detects a vertical up and down movement?

    I came across a sensor that could work for my application but it's very expensive. https://www.clrwtr.com/Products/B2N4...L60-2LI2-H1151

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,245
    Images
    27
    Rep Power
    271

    Re: Vertical movement sensor

    No, that sensor does not actually measure up-down movement. It measures inclination about one or two axes, so basically gives you the same information as a plumb bob attached to one or two protractors.

    You could get away with a single axis accelerometer if you can guarantee the sensor (and whatever it is attached to) will not be rotating about any axis (chassis rotating upward to drive up a hill). You could also try a very sensitive altimeter/pressure sensor; some of them have precision down to 1cm of air, but that makes them sensitive to interference from local airflow near the sensor.

    Your most reliable method of easily measuring vertical/altitude change is with a 9DOF IMU/AHRS sensor (like the LSM9DS1) to feed a sensor fusion filter (like the Madgwick filter (http://www.x-io.co.uk/category/open-source/)) and feed the resulting orientation quaternion plus the sensor's linear acceleration and rotational velocity into an odometry system then ignore everything that spits out except the altitude.
    Last edited by tician; 08-05-2018 at 08:37 PM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  3. #3

    Re: Vertical movement sensor

    How far up/down do you need? A barometric pressure sensor could get you approximate up/down movement.
    Of course, it would also tell you you went "up" just because a high pressure front started moving in, so it depends on environments.

    Is the location fixed? If so, any distance sensor, such as ultrasonic, infrared, or time-of-flight sensor can get you what you want. This could work for non-fixed things, too, if you need "height above whatever is below me."

    Other than that, I agree with tician, just get a 3DOF or 9DOF IMU and read out only the one of the axes you actually care about. (Or, if your sensor is rotated, use dot product to project the axis you care about.)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Hexapod in vertical surfaces
    By alvaromonty in forum Project Showcase
    Replies: 12
    Last Post: 04-26-2018, 04:41 AM
  2. Dynamixel assisted movement?
    By memmerich in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 11-04-2016, 02:46 PM
  3. Replies: 1
    Last Post: 04-10-2016, 01:34 PM
  4. HS-55 Servo problematic movement.
    By RabidCicada in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 03-25-2009, 04:57 PM
  5. suggestion to detect the jiggle movement
    By shalee21 in forum Mechanics / Construction
    Replies: 5
    Last Post: 12-15-2007, 07:36 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •