Results 1 to 4 of 4

Thread: multi versions tested still lost all tibias

  1. #1
    Join Date
    Sep 2018
    Location
    Maryland
    Posts
    11
    Rep Power
    11

    Unhappy multi versions tested still lost all tibias

    I've got vids of my PhantomX MKIII (ax18, stock arobotix board) walking with both stock code and Phoenix... freaked out a bunch of friends (and pets)

    Playing with some bad/worn cables, then after reprogramming the arbotix board, no matter which version of the Phoenix code I load, the tibias never move in any walking mode. ONLY with a 'tall' stand up.... (L6+ right joystick) will the tibias move when nearly fully standing up. If I reload the stock nuke code ,all dynamixels (including the tibias) respond as expected.

    I reload the Phoenix code.... no tibia movement while walking _parts or full , even a few old revs...of the Phoenix code no tibias! WHAT THE HECK did I do to some support file somewhere?? I've dumped and reloaded Arduino 1.6.7 and 1.8.7 environments, re-downloaded all code from github... edited the usual tibdits I 'thought' were right.... WHERE DO I START LOOKING to figure out what I messed up! (am messing up) It really makes no sense since the trossen nuke version runs fine.

    In this vid you can see the tibias working just fine while walking sideways. on the bench. inital startup after a couple re-programmings of the arbotix board ...turn on the commander it stands, with no tibia movement. L6+ right joystick to stand up tall... (legs full extension) the tibias do move a bit. So signals are there, power is there, all dimensions, horn offsets etc are as stock (on github) so what do I look for????
    really bummed here.
    <img src="http://www.nasshq.org/wizardz/hex-outside-debug2.mp4" alt="" border="0">

    ptegler

  2. #2
    Join Date
    Sep 2018
    Location
    Maryland
    Posts
    11
    Rep Power
    11

    Re: multi versions tested still lost all tibias

    wow.... no responses...found it though...stupid V2 ifdef...commented out all is well
    ptegler

  3. #3

    Re: multi versions tested still lost all tibias

    Sorry but I don't follow this forum as religiously as I used to. It feels more like a ghost town as compared to what it used to be.

    Glad you have it working

  4. #4
    Join Date
    Sep 2018
    Location
    Maryland
    Posts
    11
    Rep Power
    11

    Re: multi versions tested still lost all tibias

    not a problem. It seems this realm started around the time I started playing with uavs (fleet of 250s through 1100mm tri-bladed hexcopters) lots of autonomous sensing....seems we've all traded places now.

    I am a bit surprised though...so much material is undated...multiple revs floating around...so much ...left floating in the wind as far as dev goes.

    Search and rescue.... revamp plans for my 11kg big 1100mm 15" tri-blade hexcopter ...add hexapod legs.... fly in through canopy cover opening than walk over to survivors to deliver blankets, water etc ...but coding is sorely lacking comments and adaptability :-(

    Anyone ever put a Pixhawk (in rover mode) on a hexapod?

    yep...list come and go.... had thousands on lists I ran years back...quiet these days by comparison. Blame it on social media types lacking independent tech thought...easier to follow the masses than lead

    ptegler

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Which Python and wxPython versions for Windows for PyPose?
    By siempre.aprendiendo in forum Software and Programming
    Replies: 1
    Last Post: 08-11-2014, 06:34 PM
  2. Finaly back, a bit lost? Phidgets software.
    By Meccano Jay in forum Software and Programming
    Replies: 0
    Last Post: 09-20-2012, 10:19 AM
  3. I am so lost! Need help!
    By Tylerthomasmiller in forum DYNAMIXEL & Robot Actuators
    Replies: 18
    Last Post: 08-31-2011, 11:57 PM
  4. C# Multithreading... Ugh I'm lost here
    By nagmier in forum Software and Programming
    Replies: 6
    Last Post: 08-14-2009, 10:25 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •