Results 1 to 5 of 5

Thread: wow... how's this for a robot controller!

  1. #1

    wow... how's this for a robot controller!

    hhmmm... two joysticks similar to the Commander (EG: playstation) complete with 8 pushbuttons...but an entire computer behind it. FPV camera on a bot anda vid window via a usb receiver...your dev environment right on your controller!
    could be REAL interesting!!
    https://www.amazon.ca/Aluminum-GPD-WIN-X7-Z8750-Bluetooth/dp/B01MCV637B

    Click image for larger version. 

Name:	cool-controller1.jpg 
Views:	18 
Size:	93.4 KB 
ID:	7336

    nfi...just waiting for them to be avail!

    ptegler

  2. #2

  3. #3

    Re: wow... how's this for a robot controller!

    Cute! 5.5" screen -- that thing fits in a pocket.

    You can't really "develop" on that size keyboard, though (I've tried, with portable wireless keyboards for Raspberry Pis, at RoboGames.)

  4. #4

    Re: wow... how's this for a robot controller!

    agreed... but a usb hub, external wireless keyboard etc can change that...was thinking basically unlimited input mechanism for remote functions...can at least mod values/parameters of your code in the field while testing

    ptegler

  5. #5

    Re: wow... how's this for a robot controller!

    The competition is a Raspberry Pi with an external touchscreen, or something like that. Those are slightly cheaper, and come in separate parts, which sometimes is more advantageous (because of mounting,) and sometimes is annoying (because it's unprotected.)
    The "it's a complete package you can put in your pocket" is the nice part! And the "it runs Linux or Windows instead of Android or iOS" is the other nice part :-)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Robot Controlled by Xbox 360 Controller (Wireless)
    By No0bert in forum Robotics General Discussion
    Replies: 23
    Last Post: 01-12-2014, 04:14 PM
  2. Robot Controller, Relays, Speed Controllers
    By Parts in forum Garage Sale
    Replies: 4
    Last Post: 03-17-2012, 02:50 PM
  3. Project Robot Controller
    By Quantum in forum Project Showcase
    Replies: 20
    Last Post: 02-23-2012, 09:15 PM
  4. Handheld Robot Controller
    By jdolecki in forum Robotics General Discussion
    Replies: 1
    Last Post: 10-25-2010, 08:43 PM
  5. Question(s) PDA Controller robot design questions
    By xntx in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 05-05-2010, 04:05 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •