Results 1 to 1 of 1

Thread: Arbotix-M programmer not responding

  1. Arbotix-M programmer not responding

    Hello all, I am having trouble uploading to my new Arbotix-M. I followed the tutorials, and everything was working (i.e blink, until I tried to use the Dynamanager to set the IDs of my AX-12s. After this, I can no longer upload to my Arbotix-M. The weird thing is, with verbose output, I get the following output during the write:
    Code:
    avrdude: Version 6.3, compiled on Sep 12 2016 at 17:22:25
             Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
             Copyright (c) 2007-2014 Joerg Wunsch
    
             System wide configuration file is "/Applications/Arduino.app/Contents/Java/hardware/tools/avr/etc/avrdude.conf"
             User configuration file is "/Users/_/.avrduderc"
             User configuration file does not exist or is not a regular file, skipping
    
             Using Port                    : /dev/cu.usbserial-AI06JEWV
             Using Programmer              : arduino
             Overriding Baud Rate          : 38400
             AVR Part                      : ATmega644P
             Chip Erase delay              : 55000 us
             PAGEL                         : PD7
             BS2                           : PA0
             RESET disposition             : dedicated
             RETRY pulse                   : SCK
             serial program mode           : yes
             parallel program mode         : yes
             Timeout                       : 200
             StabDelay                     : 100
             CmdexeDelay                   : 25
             SyncLoops                     : 32
             ByteDelay                     : 0
             PollIndex                     : 3
             PollValue                     : 0x53
             Memory Detail                 :
    
                                      Block Poll               Page                       Polled
               Memory Type Mode Delay Size  Indx Paged  Size   Size #Pages MinW  MaxW   ReadBack
               ----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
               eeprom        65    10   128    0 no       2048    8      0  9000  9000 0xff 0xff
               flash         33     6   256    0 yes     65536  256    256  4500  4500 0xff 0xff
               lock           0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
               lfuse          0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
               hfuse          0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
               efuse          0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
               signature      0     0     0    0 no          3    0      0     0     0 0x00 0x00
               calibration    0     0     0    0 no          1    0      0     0     0 0x00 0x00
    
             Programmer Type : Arduino
             Description     : Arduino
             Hardware Version: 2
             Firmware Version: 1.16
             Vtarget         : 0.0 V
             Varef           : 0.0 V
             Oscillator      : Off
             SCK period      : 0.1 us
    
    avrdude: AVR device initialized and ready to accept instructions
    
    Reading | ################################################## | 100% 0.00s
    
    avrdude: Device signature = 0x1e960a (probably m644p)
    avrdude: reading input file "/var/folders/00/h70rb2456pn5rm5jdnzrdjbm020w31/T/arduino_build_496859/arbotiXBlink.ino.hex"
    avrdude: writing flash (984 bytes):
    
    Writing | avrdude: stk500_recv(): programmer is not responding
    ############avrdude: stk500_recv(): programmer is not responding
    I think this means my connection (including drivers, cable orientation, power etc) is working properly, but my programmer or bootloader isn't working properly.
    I am on a Mac using Arduino 1.6.13 with the current libraries available on Github. I have tried connecting my TX/RX pins on the cable, and can verify that they are working with the drivers (i.e text is echoed in the serial monitor). The upload says it's successful, but the program doesn't work as expected (I tried reuploading the blink example). I have tried reflashing the bootloader but it gives the same error. Does anyone have any idea what my next steps are? Or is my board fried already?

    EDIT:
    I was using an FTDI cable, also tried programming directly using a Up board as a ISP. Was able to reflash the bootloader using it, but that didn't fix the FTDI problem. Also tried flashing a script to it, but I get the verification error that other people are having.
    Last edited by raphtor; 10-17-2018 at 11:20 AM. Reason: Updated with more details

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. Dynamixel AX-12A is not responding to any command
    By masoudium in forum DYNAMIXEL & Robot Actuators
    Replies: 13
    Last Post: 02-09-2017, 12:44 PM
  2. Question(s) AX-12A + OpenCM + Monkey programmer = Servo not responding
    By OpenRobot in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 12-04-2015, 10:37 AM
  3. Question(s) MX-64AR not responding to instruction packets
    By kammce in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 04-02-2015, 12:40 PM
  4. Question(s) Dynamixel AX-12A not responding
    By patinam in forum DYNAMIXEL & Robot Actuators
    Replies: 6
    Last Post: 03-04-2013, 02:41 PM
  5. Question(s) ArbotiX Board: AVR Studio 5: Pololu USB AVR Programmer
    By dandbd in forum Software and Programming
    Replies: 5
    Last Post: 11-15-2011, 03:53 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •