Results 1 to 4 of 4

Thread: Combine MX-28 with XL-320 using r+ motion

  1. MX-28

    OpenCM using r + motion?

    I've tried it but can't, do you have a suggestion to overcome this?
    thanks
    Last edited by Elisi; 11-25-2018 at 03:49 PM.

  2. #2

    Re: Combine MX-28 with XL-320 using r+ motion

    Normally I would suggest that you ask this up on the Robotis forum, but I am pretty sure you already have.

    http://en.robotis.com/service/forum_...stx=&stx=&sfl=

    As mentioned in the other forum, you are running both as Protocol 2 and you have their voltages separate. I assume you have them both configured to run at the same Baud rate.

    Can you talk to either of them? What are you running on the OpenCM board? Is the OPenCM running the default firmware? If so is it configured for the right Buss (Serial 1 or Serial 3)...

  3. #3

    Re: Combine MX-28 with XL-320 using r+ motion

    Quick update: Looks like it was answered on the Robotis forum, saying that no you can not have multiple types of servos suing the r+ manager, as they use a Sync Write to update the motions, and these two servos do not have a common control table

  4. Re: Combine MX-28 with XL-320 using r+ motion

    Thanks KurtEck for your information, now I can know the reason why they cannot be controlled together
    Last edited by Elisi; 11-25-2018 at 03:50 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Can you use R+ Motion with HR-OS1?
    By bg404 in forum HR-OS1 Development and Discussion
    Replies: 1
    Last Post: 04-29-2015, 11:57 AM
  2. motion platform 3 DOF
    By pgerbet in forum Software and Programming
    Replies: 0
    Last Post: 07-12-2012, 04:02 AM
  3. Question(s) Motion sequencing in RoboPlus Motion?
    By jarred in forum Software and Programming
    Replies: 4
    Last Post: 05-07-2010, 09:54 AM
  4. projectile motion
    By Robo in forum Mechanics / Construction
    Replies: 3
    Last Post: 03-28-2007, 09:38 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •