Results 1 to 2 of 2

Thread: Hex M2 Nut Not fitting into Dynamixel AX-18A Servo

  1. Hex M2 Nut Not fitting into Dynamixel AX-18A Servo

    Hello All,

    I'm trying to follow the instructions at Step 4 of https://learn.trossenrobotics.com/10...bly-guide.html

    Specifically, i'm trying to slide in Hex M2 Nuts into Dynamixel AX-18A Servo but unfortunately the nuts are not fitting in. I can see the inner circle of the nut is not flush with the inner circle of the holes on the servo.

    Im afraid of hammering it in, lest i ruin or break the servo. I'm curious about a couple of things and would much appreciate help --
    1. How much pressure should I apply to the Hex M2 nut to get it into the servo? Should it involve hammering?
    2. The instructions are supposed to be for both the AX-12 and AX-18 servos but the photos show AX-12 servos, do both use the Hex M2 nut?

    Thanks!

  2. #2

    Re: Hex M2 Nut Not fitting into Dynamixel AX-18A Servo

    The AX-12 and AX-18 use the same physical size/enclosure -- the point is that you can interchange them!

    The M2 nuts should require firm but not hammering pressure to go in. It should go in with a "corner" inwards, and two "flat" sides parallel to the direction of pushing in.

    Note that nuts come in slight variation in size -- there are many standards, and many tolerance grades. If you bought the nuts yourself, you may simply have bought beefier nuts than what Robotis assumes/are using, and thus your nuts won't fit.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Not Able to Find AX-12A servo with Dynamixel Wizard
    By chenji28 in forum DYNAMIXEL & Robot Actuators
    Replies: 14
    Last Post: 12-31-2015, 12:31 AM
  2. Dynamixel servo shaking a lot - should I be worried?
    By kevining in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 01-30-2015, 11:42 PM
  3. How do I set Dynamixel servo ID using an Arduino?
    By OOrmOnIzArGoR in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 12-03-2014, 11:33 PM
  4. Question(s) Dynamixel servo- 'Deadzone'
    By vinjk in forum DYNAMIXEL & Robot Actuators
    Replies: 23
    Last Post: 07-21-2014, 05:59 AM
  5. Does Dynamixel servo AX-12 or RX-64 have motor lock mode?
    By bonmot in forum Humanoids, Walkers & Crawlers
    Replies: 6
    Last Post: 03-25-2011, 11:56 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •