Page 1 of 2 12 LastLast
Results 1 to 10 of 17

Thread: Turtlebot3 with Openmanipulator

  1. #1

    Turtlebot3 with Openmanipulator

    It seem it is being renamed the Openmanipulator-x now.
    http://emanual.robotis.com/docs/en/p...or_x/overview/
    Last edited by LloydF; 03-26-2019 at 06:35 AM.

  2. #2

    Re: Turtlebot3 with Openmanipulator

    looks like hours of entertainment

  3. #3

    Re: Turtlebot3 with Openmanipulator

    LOL. It is not even here yet and I am having issues.
    I tried to update a OpenCR board and now I have two OPenCR bricks.
    Sigh looks like hours of entertainment, starts now.

  4. #4

    Re: Turtlebot3 with Openmanipulator

    I have not done anything with mine for a few weeks now. Been busy with Puppy and with the Teensy 4 Alpha board.

    Sometimes when I had issues iwth OpenCR board, I need to revert back to using the RPI (or UP) board to reprogram the board with current default firmware, before I could get it to talk again on Arduino...

  5. #5

    Re: Turtlebot3 with Openmanipulator

    Thank you. I found page 248 in the book were you press the reset and switch 2 which forces the boot-loader to run, yea!
    That really had me thinking I bricked my boards when I noticed, I was not the only one with the same issue, so I re-read the BOOK and
    lo and behold there it was, and the only place I have ever seen mention the use of switch 2, so yea again!!

  6. #6

    Re: Turtlebot3 with Openmanipulator

    Glad that worked - Just in FYI - It is also in their e-manual...
    http://emanual.robotis.com/docs/en/p...-recovery-mode

  7. #7

    Re: Turtlebot3 with Openmanipulator

    Well with that out of the way it's back to waiting for a package .
    Look at the http://www.robotis.us/ site they have a frame set and a heavy base plate for the manipulator.
    Last edited by LloydF; 03-24-2019 at 07:44 AM.

  8. #8

    Thumbs up Re: Turtlebot3 with Openmanipulator

    Click image for larger version. 

Name:	smallbox.jpg 
Views:	131 
Size:	124.8 KB 
ID:	7443Click image for larger version. 

Name:	OpenedBox.jpg 
Views:	132 
Size:	149.9 KB 
ID:	7444Click image for larger version. 

Name:	openmanipulatorDone.jpg 
Views:	138 
Size:	117.0 KB 
ID:	7445
    Here it is. I downloaded the build instructions, as this one comes with no instructions, but useful links
    There Disclaimer really needs to be more visible. i.e Base plate is sold separately like the power supply and a controller .
    Click image for larger version. 

Name:	OpenManipulator_all_setup.jpg 
Views:	138 
Size:	48.9 KB 
ID:	7446
    The 5 Dynamixel's XM430-W350-T's come with ID's set to 11 through 15, maybe a hour and the hardware is done.
    I would install it on my turetlebot3 waffle but I must play with it, before going mobile.
    Last edited by LloydF; 03-28-2019 at 03:09 PM.

  9. #9

    Re: Turtlebot3 with Openmanipulator

    Click image for larger version. 

Name:	itisalive.jpg 
Views:	145 
Size:	110.5 KB 
ID:	7453
    The default configuration for the manipulator is on the u2d2 or a USB serial connection, and it works really well.
    They have a direct link to some STL files for 3-D printers, so I printed some motor covers to round out the sharp corners and looks more robust some how .
    Click image for larger version. 

Name:	manipulator#1.jpg 
Views:	120 
Size:	79.3 KB 
ID:	7463Click image for larger version. 

Name:	manipulator#2.jpg 
Views:	113 
Size:	91.8 KB 
ID:	7464Click image for larger version. 

Name:	manipulator#3.jpg 
Views:	113 
Size:	75.6 KB 
ID:	7465
    With a edit to the launch file the OpenCR Board runs the OpenManipulator.
    Last edited by LloydF; 03-24-2019 at 07:45 AM.

  10. #10

    Re: Turtlebot3 with Openmanipulator

    I am happy to report that I have been able to get everything working, with the exception of the RC100 joystick with the OpenManipuiator. It should work but hum I am still working on that one. I kept loading the OpenCR chain instead of:
    Go to Examples → OpenCR → 10.Etc → usb_to_dxl on Arduino IDE for OpenCR. Was making me crazy.
    It looks like there doing some good stuff with ROS Industrial for the OpenCR Board, Yea!
    http://emanual.robotis.com/docs/en/p.../#master-slave
    Last edited by LloydF; 04-06-2019 at 12:50 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. News/Announcement The Robotis TurtleBot3
    By Gort in forum Rovers
    Replies: 128
    Last Post: 08-11-2019, 05:47 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •