Results 1 to 4 of 4

Thread: How to change the speed of the AX12a and Read its current speed ?

  1. Question How to change the speed of the AX12a and Read its current speed ?

    Hi everyone,

    I am new to use dynamixel and ax12a motors. Thus, I have a few questions about ax12a. I will be very happy if you reply to this thread.

    I found these pre-defined variables from the dataset of dynamixel for ax12a to use on my code.
    AX_PRESENT_SPEED_L 38
    AX_PRESENT_SPEED_H 39

    AX_GOAL_SPEED_L 32
    AX_GOAL_SPEED_H 33

    1st Question:
    To read the current speed, I need to use this function ax12GetRegister(1,38,2); where 2 presents the byte in read mode, right ? thank you very much.

    2nd Question:
    To change the speed of the motor, I need to use this function
    ax12SetRegister2(1,32,speed_value); where this speed value is between 0 and 255 or with a different value range, right ? thank you very much.

    3rd Question:
    What is the difference between L and H (L is the Lowest Byte and H is the Highest Byte) while using in the coding and its effects on the ax12a ? thank you very much.



  2. #2

    Re: How to change the speed of the AX12a and Read its current speed ?

    The value range is documented in the manual for the servo. I don't remember the exactly values, but because it's a 2-byte register, the value range is higher than 0-255.
    The "_L" and "_H" are the two bytes that make up one 16-bit value. The full range of a 16-bit value is 0-65535, but the servo generally uses less of that range.

  3. Re: How to change the speed of the AX12a and Read its current speed ?

    Quote Originally Posted by jwatte View Post
    The value range is documented in the manual for the servo. I don't remember the exactly values, but because it's a 2-byte register, the value range is higher than 0-255.
    The "_L" and "_H" are the two bytes that make up one 16-bit value. The full range of a 16-bit value is 0-65535, but the servo generally uses less of that range.
    ax12GetRegister(1,38,2);
    ax12SetRegister2(1,32,speed_value);

    These functions are the correct formats for changing speed and getting the current speed of the motor, right ? thank you.

  4. #4

    Re: How to change the speed of the AX12a and Read its current speed ?

    With generic Robotis Servo questions, unless you are using Trossen Robotics specific hardware/software would suggest asking questions on the Robotis Forum: http://en.robotis.com/service/forum.php

    Also suggest looking at e-manual for this servo: http://emanual.robotis.com/docs/en/dxl/ax/ax-12a/

    And yes getting the present speed: http://emanual.robotis.com/docs/en/d...esent-speed-38
    on ID 38 is the correct one.

    And: http://emanual.robotis.com/docs/en/d...oving-speed-32
    is the correct one to set the moving speed.

    How this value is used may very much depend on what mode the servo is in... Again more details in the emanual

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. MX-106 speed
    By dudu2683 in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 09-22-2017, 11:57 PM
  2. Results of speed it up
    By spiked3 in forum Project Showcase
    Replies: 11
    Last Post: 07-13-2014, 06:56 AM
  3. Question(s) Looking to speed up
    By spiked3 in forum Robotics General Discussion
    Replies: 34
    Last Post: 05-02-2014, 02:34 PM
  4. Dynamixels communication speed
    By kareth in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 02-02-2014, 11:40 AM
  5. Project Large LED speed display & beam speed-traps
    By McGuireV10 in forum Projects For Request and/or Sale
    Replies: 17
    Last Post: 05-23-2009, 03:26 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •