Results 1 to 2 of 2

Thread: How can I connect ROS with Unreal engine?

  1. Post How can I connect ROS with Unreal engine?

    I recently started learning ROS and Unreal engine. Please bear my rookie mistakes and questions. Both are installed on Ubuntu 16.04.

    I am using this GitHub link to connect ROS with unreal.
    1. For the second step, I went to the repository and made a new folder named Plugin and then created another folder inside Plugin named ROSIntegration. I pasted ROSIntegration.uplugin there. After that I accessed Plugins from the Edit tab and there was no Project section in the plugin window. I created the plugin by clicking New Plugin. I finally got ROSIntegration.uplugin in the directory and unreal detected that as well and I activated it.
    2. Then it says to restart the editor and check that the code for the new plugin is built. My question is how do we check if the code is built? It isn't mentioned how that should be done.

    It feels like that connecting ROS and Unreal together isn't something for beginners but not doing it or leaving is not an option.

    If there is another easy way to do this, please tell me.

    Thank you.

  2. #2

    Re: How can I connect ROS with Unreal engine?

    I've only created Unreal plugins in Visual Studio. There, the integration is actually very nice.

    I imagine if you have an exposed function in your plugin and you can call it from Blueprint, then the code would have been built.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. News/Announcement Unreal Engine - OpenSource-Education + ROS !
    By curka in forum Robotics General Discussion
    Replies: 3
    Last Post: 09-28-2014, 06:30 PM
  2. ArbotiX Pose Engine with CM9.04
    By klims in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 09-21-2014, 02:37 AM
  3. ROS Os with Unity Engine!
    By curka in forum ROS - Robot Operating System
    Replies: 1
    Last Post: 08-31-2014, 01:09 PM
  4. Project ROS Os with Unity Engine - Possible
    By curka in forum Robotics General Discussion
    Replies: 2
    Last Post: 08-31-2014, 11:42 AM
  5. Project Compressed air engine
    By sam in forum Project Showcase
    Replies: 11
    Last Post: 09-04-2009, 12:06 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •