Results 1 to 1 of 1

Thread: Power outage when at least 8 servos are in motion

  1. Power outage when at least 8 servos are in motion

    I just put together the PhantomX MIII Hexabot with AX-18A servos and the HexabotTest checked out. Then I loaded the Phantom code onto it and was controlling it ok but every so often it would reset.

    To isolate the issue I modified the HexabotTest code to drive all the femurs and tibias down and then up simultaneously. The body is supported and no legs are touching the ground. If I do at least 4 legs at once the power cuts off briefly and it restarts.

    It works with the battery, but apparently with the power adapter the hexabot can't handle the load of at least 8 servos moving simultaneously?
    Last edited by quarkburger; 1 Week Ago at 09:42 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) How to power AX-12A servos connected to an USB2AX?
    By corot in forum DYNAMIXEL & Robot Actuators
    Replies: 6
    Last Post: 02-20-2017, 06:01 PM
  2. Replies: 15
    Last Post: 10-27-2016, 07:25 PM
  3. ax12a servos not getting power
    By deathwiz in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 04-13-2014, 06:22 PM
  4. Replies: 0
    Last Post: 12-29-2011, 10:23 AM
  5. Supplemental power for servos?
    By MaconSwift in forum Arbotix, Microcontrollers, Arduino
    Replies: 19
    Last Post: 03-05-2010, 01:36 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •