I clicked the "version 1" option when downloading R+, so I'm hoping that's good?
The "scan" button first tries a version 2 scan, which doesn't find these servos.
And the "installing firmware" log ends up saying " ... Failed" at the end. (It also has an intermediate step talking about "making sure dynamixels are active" (or "awake?")
And the firmware recovery process doesn't work -- they're not seen by the recovery mechanism.
I'll try the version 2, too, to perhaps avoid having to send them back, but the failure messages are not encouraging.
What's the right Robotis forums these days, btw? It used to be that weird Korean software in English-language mode...
Bookmarks