Results 1 to 2 of 2

Thread: SR300 Module USB

  1. #1

    SR300 Module USB

    I just placed an order for an Intel RealSense SR300 camera module and on more careful reading of the documentation realized that it does not have a standard USB connector. There is enough information in the manual to solder a hacked USB cable to the module, but I would prefer a neater solution. Anyone else have experience making a bare SR300 module work ?

    Thanks,

    JimB

  2. #2

    Re: SR300 Module USB

    Update: The module just arrived today and soldering is not an option. There are 10 conductors with a spacing of about 0.4 mm. Way too small for hand soldering. JimB

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. GPS Module for Lubuntu?
    By madelineharlow in forum Sensors
    Replies: 1
    Last Post: 12-05-2013, 01:35 PM
  2. Problem with ymal module
    By Shamma in forum ROS - Robot Operating System
    Replies: 6
    Last Post: 04-10-2011, 03:15 PM
  3. 802.11g module via SPI
    By lamont in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-21-2008, 06:51 PM
  4. Bioloid sparkfun bluetooth module
    By trey3670 in forum Humanoids, Walkers & Crawlers
    Replies: 26
    Last Post: 11-18-2008, 02:55 AM
  5. voice module for I-Droid
    By asbrandsson in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 11-28-2007, 07:09 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •