Apparently the FPV world now has a feature called "Smart Audio" to control the video transmitters, including setting output power and channel frequency.
Except it doesn't use audio at all, it uses 4800 BPS half-duplex 3.3V UART!
Also, these devices have "pit mode" where transmission power is 0.01 mW or so, meaning it can be used for bench testing without interfering with others (even at 25 mW.)
One transmitter with this feature that seems to also contain a flash card DVR on Amazon is https://amzn.to/2YHZk5k
I'm going to get one and see if it's any good. (My 832-Tx 8-channel with DIP switches is very noisy and needs replacement anyway...)
So, if we want to manage channels for the next event, this seems like a promising option!
Bookmarks