Results 1 to 2 of 2

Thread: MacBook Pro - USB desactivated when plugn FTDI-USB cable

  1. MacBook Pro - USB desactivated when plugn FTDI-USB cable

    Hello.
    I baught a Arbotix-M controller and wanted to set IDs of my Dynamixels.
    I also baught a FTDI-USB cable to can plug to my MacBook Pro (https://www.amazon.fr/gp/product/B07...?ie=UTF8&psc=1)

    Problème is that when i plug the FTDI-USB cable to my compter, Mac OS say that USB device use too many energy and is disabled. So DynaManager can never see it.
    I try to put additionnal power supply (12v:5A) to Arbotix-M controller and put the switch to "FTDI" ... the green light turn on, but the problem is the same when putting the cable to computer.

    Tonight i will try with a USB external port using external power supply but i'm not sure it can change something ...

    Anyway have seen this problem or have any idea how to fix it ?

    Thank's for help

  2. #2

    Re: MacBook Pro - USB desactivated when plugn FTDI-USB cable

    Yes the next thing I would try would be to use a powered USB HUB.

    I would also try plugging the FTDI cable into something else to make sure it's working.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Why we need to have the customized webcamera cable, not using the standard USB cable?
    By guoshihui in forum HR-OS1 Development and Discussion
    Replies: 2
    Last Post: 10-23-2015, 03:38 AM
  2. Question(s) How to disconnect the cable(s) from XL-320
    By CasperH in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 10-29-2014, 03:49 AM
  3. Question(s) Bioloid Cable = Robonova Cable?
    By xx2747 in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 09-06-2010, 06:51 PM
  4. Question(s) 2X5 to 2X7 JTAG Cable
    By LinuxGuy in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 06-09-2008, 11:00 PM
  5. interface cable
    By chocobot in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 04-10-2007, 11:04 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •