Results 1 to 4 of 4

Thread: Dynamixel AX-18A ignores commands with Arduino

  1. Unhappy Dynamixel AX-18A ignores commands with Arduino

    Hi,
    I've been using 3 servos (2 AX-18A and one AX-12A) chained with an Arduino, and it was working very well.
    However, two months after without using it, I had big issues with each : the timing has become bizarre and random. For example, when oscillating between two positions, with a one second delay between the two, the servo only moves every 5-6 seconds (to debug I only use one now).
    I've tried changing Arduino board, PC, using a new servo, downgrading Arduino, for now nothing seems to work...
    With an oscilloscope, i saw that the commands are correctly sent to the servo, so I guess it just ignores some randomly, I don't know why !
    All help appreciated!

  2. #2

    Re: Dynamixel AX-18A ignores commands with Arduino

    Hard to give any advice as there is very little data to go on.

    Example how are the servos connected to the Arduino? Which Arduino?

    What code? Are you using some libraries? Which one? Do you have a simple example that is not working?

    You might also try posting on the Robotis forum.

  3. #3
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    48

    Re: Dynamixel AX-18A ignores commands with Arduino

    Try some different wires, too, to rule that out.

  4. Re: Dynamixel AX-18A ignores commands with Arduino

    Thanks all for your help!
    Thanks to a teacher, I know the issue, a dumb one: I had forgotten to connect the Arduino's ground with the generator's, now it works like a charm!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Discussion Servo won't turn while accepting commands from an Arduino
    By ArtyTrost in forum Off Topic
    Replies: 4
    Last Post: 10-21-2017, 10:23 AM
  2. No respond from Dynamixel ax-12 using arduino
    By agha in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 08-08-2017, 09:00 AM
  3. Arduino Library for Dynamixel XL-320 (and Dynamixel PRO if modified).
    By LuisGIII in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 06-08-2015, 12:00 AM
  4. How do I set Dynamixel servo ID using an Arduino?
    By OOrmOnIzArGoR in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 12-03-2014, 11:33 PM
  5. 18 Dynamixel Ax-12A with ArbotiX/Arduino - How to connect the dynamixel?
    By Snuuq in forum Arbotix, Microcontrollers, Arduino
    Replies: 20
    Last Post: 02-14-2014, 12:29 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •