Results 1 to 2 of 2

Thread: Dynamanager finds mx-28t but not mx-106T

  1. Dynamanager finds mx-28t but not mx-106T

    Hello I am new here, I just received my first three dynamixels, and an Arbotix-m board. I was successful naming the two mx-28t motors to id 2,3. Dynamanager will not see the Mx-106T however. Wouldn't be a big problem except that because it could set the Mx-28t motors, it set the baud rate of those to 1000000, and the 106 is still at 57600. I was unable to use dynamanager 1.3 for some reason. So I had to use 1.2 from github.

    The motor responds to example code from the Artibox library, as long as I set the baud to the factory default. I either need to set the mx-28 back to factory with the new id numbers, or get the 106 into the manager. Any help would be very much appreciated.

    Trevor

  2. #2

    Re: Dynamanager finds mx-28t but not mx-106T

    Are you using "Dynamanager," or the specific "Dynamixel Manager" program that's part of the RoboPlus download?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) ArbotiX / Dynamanager problem
    By vali in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 03-20-2018, 12:01 PM
  2. Testing the MX-64T and MX-106T
    By Zenta in forum DYNAMIXEL & Robot Actuators
    Replies: 33
    Last Post: 11-13-2017, 02:20 AM
  3. Is there another app to assign motor ids besides dynamanager?
    By wthierry in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 08-15-2014, 11:38 AM
  4. Arbotix m and Dynamanager on mac
    By wthierry in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 08-12-2014, 07:15 PM
  5. Mx-106t
    By HyperCube in forum Garage Sale
    Replies: 0
    Last Post: 02-18-2013, 10:25 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •