Results 1 to 8 of 8

Thread: The Raspberry pi 4 Model B

  1. #1

    The Raspberry pi 4 Model B

    Well I have 2 of the new rpi4's with 4GB of Memory on pre-order. This will be nice.

    Raspberry Pi 4 specs

    • SoC: Broadcom BCM2711B0 quad-core A72 (ARMv8-A) 64-bit @ 1.5GHz
    • GPU: Broadcom VideoCore VI
    • Networking: 2.4 GHz and 5 GHz 802.11b/g/n/ac wireless LAN
    • RAM: 1GB, 2GB, or 4GB LPDDR4 SDRAM
    • Bluetooth: Bluetooth 5.0, Bluetooth Low Energy (BLE)
    • GPIO: 40-pin GPIO header, populated
    • Storage: microSD
    • Ports: 2 × micro-HDMI 2.0, 3.5 mm analogue audio-video jack, 2 × USB 2.0, 2 × USB 3.0, Gigabit Ethernet, Camera Serial Interface (CSI), Display Serial Interface (DSI)
    • Dimensions: 88 mm × 58 mm × 19.5 mm, 46 g
    Last edited by LloydF; 06-24-2019 at 11:54 AM.

  2. #2

    Re: The Raspberry pi 4 Model B

    Neat! Really glad they added Gigabit Ethernet.

    Are there any benchmarks on the VideoCore VI?

  3. #3

    Re: The Raspberry pi 4 Model B

    I got my first RPI4 today have the Raspberry Desktop running and am now working on ROS. Happy day's
    (Note. Tried a 1080p monitor, and this board runs way hot even with heat sinks in 4k with 3840 by 2160 or just 1080p.
    A fan is really needed here)
    Last edited by LloydF; 07-06-2019 at 01:33 PM.

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: The Raspberry pi 4 Model B

    In theory, the RPi4+4GB is more powerful than my netbook in its default configuration (2-core 1.0GHz/1.33GHz, 4GB, USB2, Fast Ethernet, 802.11n)...

    Probably will pick up one of the RPi4+4GB in the next month, or so, to see if I can get anything like my netbook performance with the RPi4 running off SD and/or USB3 thumbdrive.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. #5

    Re: The Raspberry pi 4 Model B

    If it is true that Walmart is going to carry the rpi4, this could be the pi's chance to really shine.

  6. #6
    Join Date
    Sep 2015
    Location
    Enterprise, AL
    Posts
    54
    Images
    4
    Rep Power
    20

    Re: The Raspberry pi 4 Model B

    Have you tried to get the HROS1-Framework to compile on your Pi4 yet? I've been trying to for the past few days, but not able to get all the deprecated stuff fixed to work with the latest compiler in the Pi4 OS.

  7. #7

    Re: The Raspberry pi 4 Model B

    No. Sorry I have not upgraded this robot past the rp-3, sigh!

  8. #8
    Join Date
    Sep 2015
    Location
    Enterprise, AL
    Posts
    54
    Images
    4
    Rep Power
    20

    Re: The Raspberry pi 4 Model B

    I dropped back to test a Pi3 using hros1-v3-rasbian-jessie-12-09-16.zip and everything worked in my test setup except head tracking. That was possibly just due to not having the camera plugged in.

    I did try this last week and everything failed. I later discovered/figured out, that it was due to doing update and upgrade, right away. The upgrade introduced a new version of the compiler that just will not accept a lot of deprecated things that the old compiler would. The new compiler switched those things from warnings to errors, which makes the compile fail.

    I have figured out that the compiler is what is giving me fits when I try to compile the Framework on a Pi 4. I've managed to fix, I think, the outright errors, but have a bunch of warnings still. I think I'm just down to a communications problem between the Pi 4 and the Arbotix Pro. One of the things slowing me down is having only one 12v 10A Power Supply, which means I have to turn off and disconnect from one Pi to try things on another.

    Back to troubleshooting.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX 3D Model(s) for printing
    By r3n33 in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 09-03-2015, 04:56 PM
  2. gearbox 3d model
    By sthmck in forum Mech Warfare
    Replies: 1
    Last Post: 12-11-2014, 09:54 PM
  3. MX-64- which model of Maxon motors?
    By vinjk in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 07-21-2014, 05:59 AM
  4. 3D Model Thread?
    By YoMarchYo in forum Mech Warfare
    Replies: 0
    Last Post: 04-07-2013, 03:40 AM
  5. CAD Model of Phidgets
    By cmmguy in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 04-23-2008, 04:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •